STM32N6570-D: Is XSPI/OSPI for memory only, or also external peripherals?
Does the STM32N6570-DK board support XSPI/OSPI interfaces for communication with external peripherals, or are these interfaces limited only to internal or external memory devices?
For example, if there is a Device that supports OSPI/XSPI for communication, is it possible to connect the STM32N6570-DK board to such a device to enable data exchange?
Could you please provide a clear explanation of the capabilities and practical use cases of the OSPI/XSPI interface on the STM32N6570-DK board?