Skip to main content
BRobe.3
Associate III
May 21, 2023
Question

Target Voltage Detection Fail Issue

  • May 21, 2023
  • 11 replies
  • 8196 views

Hello,

I got a stlm32 disco board. I cannot Flash.

So,I used STM32 ST-LINK UTILITY. Any connection fail even under reset. This one show Target Voltage Detection Fail. The board is powered by the USB CN2 Connector. The measurment on the CN4 Connector shows 3,3 v between 1 and 3 pins.( which seems normal)

Could this be a software issue ?

Best regards,

11 replies

NAN
Associate
June 5, 2025

My test pretty simple => a wire between pin 19 to pin 1