Skip to main content
Associate
November 22, 2024
Question

The SPI1 clock line is not working on the NUCLEO-F334R8 board

  • November 22, 2024
  • 1 reply
  • 633 views

Hi,

I am trying to get the above named board to work with an ILI9341 based display. But it is not working. I took a look at the SPI lines with a logic analyser. I saw that there was no activity on the CLOCK line. I switched to an alternative pin for the CLOCK signal but I did not get any result.

What could be wrong? Please find attached a copy of my project files for you to take a look at.

Thank you.

1 reply

Andrew Neil
Super User
November 22, 2024

Have you checked the board's User Manual and/or schematics to see if there is anything else using that pin?

Can you toggle that pin just as a basic GPIO?

 


@mubarrakky wrote:

I saw that there was no activity on the CLOCK line.


Is there any activity on any other line(s) ?

Please post the schematic of how you are connecting the "ILI9341 based display"

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
November 22, 2024

1. I checked illustration in the STM32CubeIDE (see the picture below). There's a green LED called LD2 using that CLOCK LINE.

2. I can toggle the PIN as a basic GPIO.

3. There was activity on the MOSI, MISO and CS line.

4. This is as close to a schematic as I can get (see the picture below). I attached the updated code to this post. Let me know if you need any other info.

mubarrakky_0-1732294528086.png

The display is being powered by +3.3V and GND.

mubarrakky_1-1732296483434.png

Screenshot of the SPI signals.