Skip to main content
Associate III
May 24, 2024
Solved

UART Communication - STM32H745I-DISCO via ST-LINK

  • May 24, 2024
  • 2 replies
  • 1473 views

Hey everyone,

I want an UART communication between my PC and my STM32H745 Disco board. 

By default the UART 3 (connected to STLINK connector) is one core M4. 

My baud rate is 115200. My pins are initialized by default. 

My main is this :

fru999_0-1716556054580.png

and the hal_uart_transmit function returns HAL_OK.
On my computer, with Putty, i can't see the data sent. 

Can you help me with this ? :)

 

 

Best answer by fru999

Pin pour UART 3 sur STM32H745 DISCO sont :

TX : PB10 

RX : PC11

 

2 replies

KDJEM.1
Technical Moderator
May 24, 2024

Hello @fru999 ,

Please make sure that the UART configuration in your code matches the settings in Putty: baud rate, word length, parity.

Could you please take a look at this wiki: Step3 Introduction to the UART may help.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
fru999AuthorBest answer
Associate III
May 24, 2024

Pin pour UART 3 sur STM32H745 DISCO sont :

TX : PB10 

RX : PC11