Skip to main content
OMekk
Visitor II
July 14, 2024
Question

using CN5 in STLINK-V3MODS

  • July 14, 2024
  • 1 reply
  • 1014 views

Hello,

I have an STLINK-V3MODS debugger, and I want to solder the 14-pin target JTAG socket. I see that there are messing components around when comparing the file "UM2502" page 13, Figure 7. MB1467 top layout to my real debugger. I see lots of missing components around. If there are some missing components that I need to populate, could you please provide me with the required components ?

OMekk_0-1720988910842.png

OMekk_1-1720989062563.png

3381462-40.jpg

 

Thank you,

BR,

 

1 reply

KDJEM.1
Technical Moderator
August 7, 2024

Hello @OMekk ,

JTAG protocol is a Debug/Program protocol used for STM32 microcontrollers. This function is available on CN2
(STLINK-V3MODS) and CN5 (STLINK-V3MINI).

KDJEM1_0-1723026051216.png

 

The "Voltage Translator reference design for STLINK-V3MODS" document has the reference to connect an external STDC14 connector to the STLINK-V3MODS board.

Is my reply answer your request?

 

Thank you for your contribution in STCommunity.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.