Skip to main content
Andrew Neil
Super User
September 18, 2024
Question

What do Linux (and Mac?) people call a "Virtual COM Port" ?

  • September 18, 2024
  • 2 replies
  • 1110 views

So a bit off-topic, but arose in the context of STM32 Nucleo boards:

https://community.st.com/t5/stm32-mcus-products/communication-between-nucleo-f411re-and-raspberry-pi-using-st/m-p/721571

 

"Virtual COM Port" is a Windows-centric term - referring to the COMx: device names that Windows assigns to Async Serial interfaces.

Linux doesn't have COMx: devices  - instead, it has /dev/ttyXXX 

I know nothing about Mac.

So what do Linux people call a "Virtual COM Port" ?

Do they just say "Virtual COM Port" - ignoring the Windows connotation, and knowing that it really means a /dev/tty device?

Or do they have another recognised name for the concept?

2 replies

Pavel A.
Super User
September 18, 2024

/dev/ttyACM, /dev/ttyUSB ... and so on. On Mac OS: /dev/tty.usb... something like this.

On Windows the COMx names are deprecated. Serial port devices are recognized by having specific interface class ID. TL;DR there is API that lists all devices of this class and returns the "file name"  to open.

 

Andrew Neil
Super User
September 18, 2024

Yes, but when speaking about it, what word(s) do they use?

 

The ST documentation uses "Virtual COM Port" pretty much exclusively, I think - so Windows-centric:

AndrewNeil_0-1726675383241.png

AndrewNeil_1-1726675406219.png

AndrewNeil_2-1726675421796.png

But what would a die-hard Linux person write there?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
September 18, 2024

Not a die-hard, I mostly describe using /dev/tty , but CDC or ACM is also quite common

ACM is a generic USB class driver for a modem, so ttyACMx

CDC is USB communications device class

As Pavel points out ttyUSBx also high up there in what will enumerate

Depends on the specific equipment and how it presents itself, seen GPS/GNSS USB G-Mouse/Mice com up as ttyACM and ttyUSB

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
mƎALLEm
Technical Moderator
September 18, 2024

I think it's called Virtual Serial Port.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."