Why is the rated supply voltage for the 5V pin regulator on the bluepill datasheet 4.0v and not 5v?
I would like to know whether the stm32f103c8t6(Blue pill) can be supplied using a 5v source through the regulator ( 5V pin); I've seen a lot of people indicate that it was possible but the datasheet clearly says that the maximum voltage the regulator can take is 4.0v. In addition, I've read that the regulator is disabled in stop mode, does that mean that I cannot use my external 5v source in while in stop mode? and is the onboard usb regulator the same one used on the 5v pin? ( I've only seen one regulator in the blue pill schematic)
Image to see what portion of the datasheet I'm referring to :