Skip to main content
Associate
December 9, 2024
Question

X-NUCLEO-IKS4A1 and X-NUCLEO-WB05KN1 Compatibility

  • December 9, 2024
  • 2 replies
  • 1975 views

Hi,

I am trying to make both IKS4A1 and WB05KN1 (see datasheet attached) shields work together on a NUCLEO-U575ZI.

Using the example projects I can use both separately. I used the SensorDemo_BLESensor-App from X-CUBE-WB05N (https://www.st.com/en/embedded-software/x-cube-wb05n.html) with the WB05KN1 and DataLogTerminal from X-CUBE-MEMS1 (https://www.st.com/en/embedded-software/x-cube-mems1.html).

I then try to plug both shields on the Nucleo board. I mounted the WB05KN1 on top of the IKS4A1. My first step was just to flash the board with the SensorDemo_BLESensor-App to see if it was still working. Unfortunately it is not.

I spend several hours trying to find the issue. I suspect a pin conflict but reading the documentations, I was not able to find the problem.I also notice that in this configuration the DataLogTerminal project is working.

I used STM32CubeIDE.

Could someone please help me?

 

2 replies

Technical Moderator
December 9, 2024

Hello @RemHi ,

Did you try with the latest release of STM32CubeProgrammer tool?

What exactly did the error message say?

Please share your log of the sequence when you tried to flash the board?

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
RemHiAuthor
Associate
December 9, 2024

Maybe I wasn't clear. I do not have issue flashing the board. I can make the WB05KN1 working on the nucleo board when mounted alone. But when I also mount the IKS4A1, its not working anymore (I didn't change anything in the binary used to flash the nucleo board).

Andrew Neil
Super User
December 9, 2024

@RemHi wrote:

I suspect a pin conflict but reading the documentations, I was not able to find the problem?


It's here:

AndrewNeil_1-1733752953479.png

AndrewNeil_2-1733752972069.png

 

Both the NUCLEO-U575ZI-Q and the X-NUCLEO-WB05KN1 are driving their VCP onto the Arduino D0-D1 pins.

You're going to have to disable one of them.

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
RemHiAuthor
Associate
December 9, 2024

As long as I understood, these pins are used for the UART communications between the NUCLEO-U575ZI-Q and the X-NUCLEO-WB05KN1.

In my mind this can't be the problem because when mounted alone on the NUCLEO-U575ZI-Q, I could used the X-NUCLEO-WB05KN1 (using the SensorDemo_BLESensor-App example project). I used ST BLE Sensor APP for smartphone and I could see the bluetooth signal and received data.

I only got a problem when I add the IKS4A1 shield between the X-NUCLEO-WB05KN1 and the NUCLEO-U575ZI-Q. It seems not to work anymore (still using SensorDemo_BLESensor-App) = with ST BLE Sensor I can't see anymore the bluetooth signal.

 

 

Andrew Neil
Super User
December 9, 2024

@RemHi wrote:

As long as I understood, these pins are used for the UART communications between the NUCLEO-U575ZI-Q and the X-NUCLEO-WB05KN1.


Ah yes, my mistake - they are swapped TX-RX and RX-TX.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.