Skip to main content
Senior III
August 22, 2025
Solved

ADC not working maybe a timer issue?

  • August 22, 2025
  • 1 reply
  • 288 views

NUCLEO-F411RE

I am trying to read data from a ADXL1002Z.

I have set up my board to use PA1 (A1 on the Arduino header) as ADC1_1

/* adc.h */
#ifndef INC_ADC_H_
#define INC_ADC_H_

#include <stdint.h>

void pa1_adc_init(void);
uint32_t adc_read(void);

void start_conversion(void);

#endif /* ADC_H_ */

 

and...

#include "stm32f4xx.h"

#include "adc.h"

#define GPIOAEN		(1U<<0)
#define ADC1EN		(1U<<8)
#define ADC_CH1		(1U<<0)
#define ADC_SEQ_LEN_1	 0x00
#define CR2_AD0N	(1U<<0)
#define CR2_SWSTART	(1U<<30)
#define CR2_CONT	(1U<<1)
#define CR1_EOCIE	(1U<<5)
#define SR_EOC (1U<<1)

void pa1_adc_init(void)
{
	/***Configure the ADC GPIO pin ***/
	/*Enable clock access to GPIOA*/
	RCC->AHB1ENR |= GPIOAEN;

	/*Set the mode of PA1 to analog*/
	GPIOA->MODER |=(1U<<2);
	GPIOA->MODER |=(1U<<3);

	/***Configure the ADC module***/
	/*Enable clock access to ADC */
	RCC->APB2ENR |= ADC1EN;

	/*Conversion sequence start*/
	ADC1->SQR3 = ADC_CH1;

	/*Conversion sequence length*/
	ADC1->SQR1 = ADC_SEQ_LEN_1;

	/*Enable ADC module*/
	ADC1->CR2 |= CR2_AD0N;
}

void start_conversion(void)
{
	/*Enable continuous conversion*/
	ADC1->CR2 |= CR2_CONT;

	/*Start adc conversion*/
	ADC1->CR2 |= CR2_SWSTART;
}

uint32_t adc_read(void)
{
	/*Wait for conversion to be complete*/
	while(!(ADC1->SR & SR_EOC)){}

	/*Read converted result*/
	return (ADC1->DR);
}

 

Use in `main.c`

 

// I am using a HAL UART & stdio hence the use of printf

#include "adc.h"

uint16_t g_sensor_value;

main()
{
 pa1_adc_init();
 start_conversion();

 while(1)
 {
 g_sensor_value = adc_read();
 printf("%d,\n", (int)g_sensor_value);
 HAL_Delay(500); 
 }

} 


I just get noise around the same level from the sensor regardless of its orientation. To test of the ADC was working I put a jumper from PA1 (A1 on the board header) to GND on the board & nothing changed, still the same noise at the same level, connected to 3.3V, still no change.

 

I have FreeRTOS running that has control over SysTick. To get the HAL_UART working I had to change System Core -> SYS -> Timebase Source to TIM1.
Was this a mistake? Is this affecting how ADC1_1 is behaving?


 

Best answer by NicRoberts

OK after a day & half trying to debug this. I just needed a delay after the print()

 

 

1 reply

NicRobertsAuthorBest answer
Senior III
August 22, 2025

OK after a day & half trying to debug this. I just needed a delay after the print()