Skip to main content
Associate II
June 10, 2025
Question

ADC SampleRate

  • June 10, 2025
  • 1 reply
  • 288 views

I wonder why I have data in the buffer when my sample rate is 30KHz and 0 when the sample rate is 50KHz.

f99145d781a5fcb8359072aa8206816.png
f1be29b49f1cb0445c3628c3ac7be42.png

 

b165ac61fbe58954536a4774397358b.png

cee005af684f9800dd5c4568c02061d.png

44ade4a41c9f3f4e07ea463d79104d2.png

8ab135ed9500848d02bf1e3b02945af.png


My code:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "adc.h"
#include "dac.h"
#include "dma.h"
#include "spi.h"
#include "tim.h"
#include "usart.h"
#include "gpio.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
//#include "AD9833.h"
// #include "Key.h" 
// #include "LCD.h"
// #include "LowPowerCtrl.h"
// // #include "stm32f4xx_hal_rcc.h"
// #include "SignalGenerator.h"
// #include "SignalSampling.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */
#define ADC1_TRIGGER htim3

uint8_t ADC1_CompleteFlag = 0; // ADC1转换完成标志位
uint8_t ADC2_CompleteFlag = 0; // ADC2转换完成标志位

#define ADC_TIM_Clock 84e6 // 定时器时钟频率

#define ADC_BUFFER_SIZE 1024 // 假设采2048组数据(FFT一般要2的幂次)

#define ADC_SampleRate 30e3

uint32_t adc_buffer[ADC_BUFFER_SIZE]; // 注意是uint32_t,因为双ADC打包成32位

uint16_t adc_buffer1[ADC_BUFFER_SIZE]; 
uint16_t adc_buffer2[ADC_BUFFER_SIZE]; 


void ADC_SetSampleRate(TIM_HandleTypeDef *htim, float sample_rate)
{
 uint32_t Timer_Clock = ADC_TIM_Clock / (htim->Instance->PSC + 1);
 uint32_t timer_reload_value = (uint32_t)(Timer_Clock / sample_rate) - 1;
 if (timer_reload_value < 1) timer_reload_value = 1;

 HAL_TIM_Base_Stop(htim); // 安全:暂停 TIM
 __HAL_TIM_SET_AUTORELOAD(htim, timer_reload_value);
 __HAL_TIM_SET_COUNTER(htim, 0); // 重置计数器
 HAL_TIM_Base_Start(htim); // 重新启动 TIM

 USART_Printf(&huart1, "ADC TimerClock=%lu, ARR=%lu, SampleRate=%.1f Hz\r\n",
 Timer_Clock, timer_reload_value, sample_rate);
}


/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_SPI1_Init();
 MX_USART1_UART_Init();
 MX_TIM2_Init();
 MX_TIM1_Init();
 MX_ADC1_Init();
 MX_ADC2_Init();
 MX_DAC_Init();
 MX_TIM3_Init();
 MX_TIM4_Init();
 MX_TIM5_Init();
 MX_TIM6_Init();
 /* USER CODE BEGIN 2 */





 ADC_SetSampleRate(&ADC1_TRIGGER,ADC_SampleRate);
 HAL_ADC_Start(&hadc2);
 HAL_ADCEx_MultiModeStart_DMA(&hadc1,adc_buffer,ADC_BUFFER_SIZE);
 HAL_TIM_Base_Start(&ADC1_TRIGGER);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {


 if(ADC1_CompleteFlag == 1)
 {
 

 for(uint16_t i = 0 ; i< ADC_BUFFER_SIZE ; i++)
 {
 adc_buffer1[i] = (adc_buffer[i] & 0x0000FFFF);
 adc_buffer2[i] = (adc_buffer[i] & 0xFFFF0000) >> 16;

 // USART_Printf(&huart1,"%d,%d,%d\n",adc_buffer[i],adc_buffer1[i],adc_buffer2[i]);
 // USART_Printf(&huart1,"%d,%d\n",adc_buffer1[i],adc_buffer2[i]);
 //USART_Printf(&huart1,"%d\n",adc_buffer2[i]);
 }
 
 ADC1_CompleteFlag = 0;
 }
 



 
 // Key_Process(); 

 // HAL_Delay(10); 




 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enables the Clock Security System
 */
 HAL_RCC_EnableCSS();
}

/* USER CODE BEGIN 4 */


void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
 if(hadc == &hadc1)
 {
 HAL_TIM_Base_Stop(&ADC1_TRIGGER);
 // USART_Printf(&huart1,"ADC Complete!\n");
 ADC1_CompleteFlag = 1; // 

 }

}


// void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
// {
// if(htim == &ADC1_TRIGGER)
// {
// // USART_Printf(&huart1, "ADC_Timer Interrupt\n");
// }

// if(htim == &htim5)
// {


// }

// if(htim == &htim6)
// {
 
// }
// }

 // while(HAL_GPIO_ReadPin(WKUP_GPIO_Port,WKUP_Pin) == GPIO_PIN_SET); 

 // if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB)) 
 // { 
 // USART_Printf(&huart1,"IF:SB:%d WU:%d\n",__HAL_PWR_GET_FLAG(PWR_FLAG_SB),__HAL_PWR_GET_FLAG(PWR_FLAG_WU));
 // __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); // 
 // __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); // 
 
 // }

 // HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
 // USART_Printf(&huart1,"SB:%d WU:%d\n",__HAL_PWR_GET_FLAG(PWR_FLAG_SB),__HAL_PWR_GET_FLAG(PWR_FLAG_WU));


// define:
// #define ADC_BUFFER_SIZE 1024 // 假设采2048组数据(FFT一般要2的幂次)
// uint32_t adc_buffer[ADC_BUFFER_SIZE]; // 注意是uint32_t,因为双ADC打包成32位
// uint16_t adc_buffer1[ADC_BUFFER_SIZE]; 
// uint16_t adc_buffer2[ADC_BUFFER_SIZE]; 
// #define ADC1_TRIGGER htim3
// #define ADC_TIM_Clock 84e6
// #define ADC_SampleRate 10e3
// void ADC_SetSampleRate(TIM_HandleTypeDef *htim, float sample_rate)
// {
// uint32_t Timer_Clock = ADC_TIM_Clock / (htim->Instance->PSC + 1);
// uint32_t timer_reload_value = (uint32_t)(Timer_Clock / sample_rate) - 1;
// if (timer_reload_value < 1) timer_reload_value = 1;

// HAL_TIM_Base_Stop(htim); // 安全:暂停 TIM
// __HAL_TIM_SET_AUTORELOAD(htim, timer_reload_value);
// __HAL_TIM_SET_COUNTER(htim, 0); // 重置计数器
// HAL_TIM_Base_Start(htim); // 重新启动 TIM

// USART_Printf(&huart1, "ADC TimerClock=%lu, ARR=%lu, SampleRate=%.1f Hz\r\n",
// Timer_Clock, timer_reload_value, sample_rate);
// }

// // int main()
// ADC_SetSampleRate(&ADC1_TRIGGER,ADC_SampleRate);
// HAL_ADC_Start(&hadc2);
// HAL_ADCEx_MultiModeStart_DMA(&hadc1,adc_buffer,ADC_BUFFER_SIZE);
// HAL_TIM_Base_Start(&ADC1_TRIGGER);
// while (1)
// {


// if(ADC1_CompleteFlag == 1)
// {
// for(uint16_t i = 0 ; i< ADC_BUFFER_SIZE ; i++)
// {
// adc_buffer1[i] = (adc_buffer[i] & 0x0000FFFF);
// adc_buffer2[i] = (adc_buffer[i] & 0xFFFF0000) >> 16;

// //USART_Printf(&huart1,"%d,%d,%d\n",adc_buffer[i],adc_buffer1[i],adc_buffer2[i]);
// //USART_Printf(&huart1,"%d,%d\n",adc_buffer1[i],adc_buffer2[i]);
// USART_Printf(&huart1,"%d\n",adc_buffer2[i]);
// }
// ADC1_CompleteFlag = 0;
// }
// }

 
// void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
// {
// if(hadc == &hadc1)
// {
// ADC1_CompleteFlag = 1; // 设置ADC1转换完成标志位

// }

// }
// ADC TimerClock=84000000, ARR=8399, SampleRate=10000.0 Hz
// ADC TimerClock=84000000, ARR=2099, SampleRate=40000.0 Hz
// ADC TimerClock=84000000, ARR=1679, SampleRate=50000.0 Hz

// 为什么采样率设置为50K时,主循环没有打印串口数据,DMA是normal模式,排除串口速度跟不上
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */



ADC:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file adc.c
 * @brief This file provides code for the configuration
 * of the ADC instances.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "adc.h"

/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

ADC_HandleTypeDef hadc1;
ADC_HandleTypeDef hadc2;
DMA_HandleTypeDef hdma_adc1;

/* ADC1 init function */
void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T3_TRGO;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_DUALMODE_REGSIMULT;
 multimode.DMAAccessMode = ADC_DMAACCESSMODE_2;
 multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_8;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_15CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}
/* ADC2 init function */
void MX_ADC2_Init(void)
{

 /* USER CODE BEGIN ADC2_Init 0 */

 /* USER CODE END ADC2_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC2_Init 1 */

 /* USER CODE END ADC2_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc2.Init.Resolution = ADC_RESOLUTION_12B;
 hadc2.Init.ScanConvMode = DISABLE;
 hadc2.Init.ContinuousConvMode = DISABLE;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.NbrOfConversion = 1;
 hadc2.Init.DMAContinuousRequests = DISABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_9;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_15CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC2_Init 2 */

 /* USER CODE END ADC2_Init 2 */

}

void HAL_ADC_MspInit(ADC_HandleTypeDef* adcHandle)
{

 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(adcHandle->Instance==ADC1)
 {
 /* USER CODE BEGIN ADC1_MspInit 0 */

 /* USER CODE END ADC1_MspInit 0 */
 /* ADC1 clock enable */
 __HAL_RCC_ADC1_CLK_ENABLE();

 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**ADC1 GPIO Configuration
 PB0 ------> ADC1_IN8
 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* ADC1 DMA Init */
 /* ADC1 Init */
 hdma_adc1.Instance = DMA2_Stream0;
 hdma_adc1.Init.Channel = DMA_CHANNEL_0;
 hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
 hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_adc1.Init.Mode = DMA_NORMAL;
 hdma_adc1.Init.Priority = DMA_PRIORITY_LOW;
 hdma_adc1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(adcHandle,DMA_Handle,hdma_adc1);

 /* USER CODE BEGIN ADC1_MspInit 1 */

 /* USER CODE END ADC1_MspInit 1 */
 }
 else if(adcHandle->Instance==ADC2)
 {
 /* USER CODE BEGIN ADC2_MspInit 0 */

 /* USER CODE END ADC2_MspInit 0 */
 /* ADC2 clock enable */
 __HAL_RCC_ADC2_CLK_ENABLE();

 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**ADC2 GPIO Configuration
 PB1 ------> ADC2_IN9
 */
 GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /* USER CODE BEGIN ADC2_MspInit 1 */

 /* USER CODE END ADC2_MspInit 1 */
 }
}

void HAL_ADC_MspDeInit(ADC_HandleTypeDef* adcHandle)
{

 if(adcHandle->Instance==ADC1)
 {
 /* USER CODE BEGIN ADC1_MspDeInit 0 */

 /* USER CODE END ADC1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_ADC1_CLK_DISABLE();

 /**ADC1 GPIO Configuration
 PB0 ------> ADC1_IN8
 */
 HAL_GPIO_DeInit(GPIOB, GPIO_PIN_0);

 /* ADC1 DMA DeInit */
 HAL_DMA_DeInit(adcHandle->DMA_Handle);
 /* USER CODE BEGIN ADC1_MspDeInit 1 */

 /* USER CODE END ADC1_MspDeInit 1 */
 }
 else if(adcHandle->Instance==ADC2)
 {
 /* USER CODE BEGIN ADC2_MspDeInit 0 */

 /* USER CODE END ADC2_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_ADC2_CLK_DISABLE();

 /**ADC2 GPIO Configuration
 PB1 ------> ADC2_IN9
 */
 HAL_GPIO_DeInit(GPIOB, GPIO_PIN_1);

 /* USER CODE BEGIN ADC2_MspDeInit 1 */

 /* USER CODE END ADC2_MspDeInit 1 */
 }
}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

 

1 reply

KnarfB
Super User
June 10, 2025

For small Timer_Clock  and high sample_rate, (uint32_t)(Timer_Clock / sample_rate) will be zero. Subtracting 1 yields an overflow because of unsigned, which results in a huge number. This may effectively stop your ADC capture.

hth

KnarfB