Skip to main content
TheRaprus
Associate III
May 19, 2025
Question

AntiTamper doesn't work in examples and new programs

  • May 19, 2025
  • 3 replies
  • 501 views

Hi to everybody.

I'm trying to create a simple program testing the anti tamper function of the STM32 serie U0.

I have the Nucleo U031, but I have tested with the U083's example (adjusted in the MCU tipe) but nothing changes, both LL and HAL. (there are different examples using LL and HAL, but only for U083 version).

Create a new HAL project using the U031 but the pressing of the blue button (connected to the PC13) doesn't work.

The new self create project is exaclty = to the example, but nothing.

Using another Nucleo such as L073 and create a new project from scratch work.
Simply, I have enabled the RTC_Tamp IRQ from NVIC, put a breakpoint in the ISR but nothing.

Where is the problem?

3 replies

May 19, 2025

Double-check the EXTI configuration for the tamper line. Even if the NVIC interrupt is enabled, the external interrupt might not be routed correctly from the tamper event.

TheRaprus
TheRaprusAuthor
Associate III
May 19, 2025

Donnow how to do it: simply enable it from CubeMX:

2025-05-19_14h09_29.png

Nothing else to do. Or I donnow where I can add some other settings.
Moreover, why the ST example doesn't work too?

TheRaprus
TheRaprusAuthor
Associate III
May 26, 2025

Any news? Still stuck on this.

Moreover, the HAL U083 example doesn't generate the ISR as my solution for 031 do.