Skip to main content
Associate II
October 9, 2025
Question

Can't open my flash memory on Windows

  • October 9, 2025
  • 3 replies
  • 384 views

Hello,

I am trying to set up an external flash memory (MX25V1635F) on a Nucleo-U575ZI-Q.
I have successfully used the low-level drivers (LLD) from the manufacturer Macronix and integrated them into the Levelx functions. (more info : https://community.st.com/t5/stm32-mcus-embedded-software/difficulties-using-fx-media-format/td-p/845435 )
Also, i use FileX to formand open my media, and it seems to work : 

 UINT ret = FX_SUCCESS;
 /* USER CODE BEGIN MX_FileX_Init */
 lx_stm32_nor_custom_driver_initialize(&nor_flash);

 /* USER CODE END MX_FileX_Init */

 /* Initialize FileX. */
 fx_system_initialize();

 /* USER CODE BEGIN MX_FileX_Init 1*/

 /* Format the NOR flash as FAT */
	 status = fx_media_format(&nor_flash_disk,
	 fx_stm32_levelx_nor_driver, // Driver entry
	 (VOID*)NOR_CUSTOM_DRIVER_ID, // Device info pointer
								(UCHAR*)media_memory, // Media buffer pointer
	 sizeof(media_memory), // Media buffer size
	 "NOR_FLASH_DISK", // Volume Name
	 1, // Number of FATs
	 32, // Directory Entries
	 0, // Hidden sectors
								TOTAL_SECTOR_LOGICAL,		 // Total sectors
								SECTOR_SIZE_LOGICAL, // Sector size
	 8, // Sectors per cluster
	 1, // Heads
	 1); // Sectors per track
 /* Check if the format status */
 if (status != FX_SUCCESS)
 {
 Error_Handler();
 }

 /* Open the SPI NOR Flash disk driver. */
 status = fx_media_open(&nor_flash_disk, "FX_LX_NOR_DISK", fx_stm32_levelx_nor_driver,(VOID*)NOR_CUSTOM_DRIVER_ID , media_memory, sizeof(media_memory));
 /* Check the media open status. */
 if (status != FX_SUCCESS)
 {
 Error_Handler();
 }


I'm using USBX as Device and MSC : 

UINT MX_USBX_Device_Init(VOID)
{
 UINT ret = UX_SUCCESS;
 UCHAR *device_framework_high_speed;
 UCHAR *device_framework_full_speed;
 ULONG device_framework_hs_length;
 ULONG device_framework_fs_length;
 ULONG string_framework_length;
 ULONG language_id_framework_length;
 UCHAR *string_framework;
 UCHAR *language_id_framework;

 UCHAR *pointer;

 /* USER CODE BEGIN MX_USBX_Device_Init0 */

 /* USER CODE END MX_USBX_Device_Init0 */
 pointer = ux_device_byte_pool_buffer;

 /* Initialize USBX Memory */
 if (ux_system_initialize(pointer, USBX_DEVICE_MEMORY_STACK_SIZE, UX_NULL, 0) != UX_SUCCESS)
 {
 /* USER CODE BEGIN USBX_SYSTEM_INITIALIZE_ERROR */
 return UX_ERROR;
 /* USER CODE END USBX_SYSTEM_INITIALIZE_ERROR */
 }

 /* Get Device Framework High Speed and get the length */
 device_framework_high_speed = USBD_Get_Device_Framework_Speed(USBD_HIGH_SPEED,
 &device_framework_hs_length);

 /* Get Device Framework Full Speed and get the length */
 device_framework_full_speed = USBD_Get_Device_Framework_Speed(USBD_FULL_SPEED,
 &device_framework_fs_length);

 /* Get String Framework and get the length */
 string_framework = USBD_Get_String_Framework(&string_framework_length);

 /* Get Language Id Framework and get the length */
 language_id_framework = USBD_Get_Language_Id_Framework(&language_id_framework_length);

 /* Install the device portion of USBX */
 if (ux_device_stack_initialize(device_framework_high_speed,
 device_framework_hs_length,
 device_framework_full_speed,
 device_framework_fs_length,
 string_framework,
 string_framework_length,
 language_id_framework,
 language_id_framework_length,
 UX_NULL) != UX_SUCCESS)
 {
 /* USER CODE BEGIN USBX_DEVICE_INITIALIZE_ERROR */
 return UX_ERROR;
 /* USER CODE END USBX_DEVICE_INITIALIZE_ERROR */
 }

 /* Initialize the storage class parameters for the device */
 storage_parameter.ux_slave_class_storage_instance_activate = USBD_STORAGE_Activate;
 storage_parameter.ux_slave_class_storage_instance_deactivate = USBD_STORAGE_Deactivate;

 /* Store the number of LUN in this device storage instance */
 storage_parameter.ux_slave_class_storage_parameter_number_lun = STORAGE_NUMBER_LUN;

 /* Initialize the storage class parameters for reading/writing to the Flash Disk */
 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_last_lba = USBD_STORAGE_GetMediaLastLba();

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_block_length = USBD_STORAGE_GetMediaBlocklength();

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_type = 0;

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_removable_flag = STORAGE_REMOVABLE_FLAG;

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_read_only_flag = STORAGE_READ_ONLY;

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_read = USBD_STORAGE_Read;

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_write = USBD_STORAGE_Write;

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_flush = USBD_STORAGE_Flush;

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_status = USBD_STORAGE_Status;

 storage_parameter.ux_slave_class_storage_parameter_lun[0].
 ux_slave_class_storage_media_notification = USBD_STORAGE_Notification;

 /* USER CODE BEGIN STORAGE_PARAMETER */

 /* USER CODE END STORAGE_PARAMETER */

 /* Get storage configuration number */
 storage_configuration_number = USBD_Get_Configuration_Number(CLASS_TYPE_MSC, 0);

 /* Find storage interface number */
 storage_interface_number = USBD_Get_Interface_Number(CLASS_TYPE_MSC, 0);

 /* Initialize the device storage class */
 if (ux_device_stack_class_register(_ux_system_slave_class_storage_name,
 ux_device_class_storage_entry,
 storage_configuration_number,
 storage_interface_number,
 &storage_parameter) != UX_SUCCESS)
 {
 /* USER CODE BEGIN USBX_DEVICE_STORAGE_REGISTER_ERROR */
 return UX_ERROR;
 /* USER CODE END USBX_DEVICE_STORAGE_REGISTER_ERROR */
 }

 /* USER CODE BEGIN MX_USBX_Device_Init1 */
 MX_USB_OTG_FS_PCD_Init();

 HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_FS, 0x80);
 HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 0, USBD_MAX_EP0_SIZE / 4);
 HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 1, USBD_MSC_EPIN_FS_MPS / 2);

 if(ux_dcd_stm32_initialize((ULONG)USB_OTG_FS, (ULONG)&hpcd_USB_OTG_FS) != UX_SUCCESS)
 {
 Error_Handler();
 }
 HAL_PCD_Start(&hpcd_USB_OTG_FS);
 /* USER CODE END MX_USBX_Device_Init1 */

 return ret;
}


And i'm using this function for MSC :

VOID USBD_STORAGE_Activate(VOID *storage_instance)
{
 /* USER CODE BEGIN USBD_STORAGE_Activate */
 UX_PARAMETER_NOT_USED(storage_instance);
 /* USER CODE END USBD_STORAGE_Activate */

 return;
}

/**
 * @brief USBD_STORAGE_Deactivate
 * This function is called when extraction of a storage device.
 * @PAram storage_instance: Pointer to the storage class instance.
 * @retval none
 */
VOID USBD_STORAGE_Deactivate(VOID *storage_instance)
{
 /* USER CODE BEGIN USBD_STORAGE_Deactivate */
 UX_PARAMETER_NOT_USED(storage_instance);
 /* USER CODE END USBD_STORAGE_Deactivate */

 return;
}

/**
 * @brief USBD_STORAGE_Read
 * This function is invoked to read from media.
 * @PAram storage_instance : Pointer to the storage class instance.
 * @PAram lun: Logical unit number is the command is directed to.
 * @PAram data_pointer: Address of the buffer to be used for reading or writing.
 * @PAram number_blocks: number of sectors to read/write.
 * @PAram lba: Logical block address is the sector address to read.
 * @PAram media_status: should be filled out exactly like the media status
 * callback return value.
 * @retval status
 */
UINT USBD_STORAGE_Read(VOID *storage_instance, ULONG lun, UCHAR *data_pointer,
 ULONG number_blocks, ULONG lba, ULONG *media_status)
{
 UINT status = UX_SUCCESS;

 /* USER CODE BEGIN USBD_STORAGE_Read */
 UINT fx_status;

 UX_PARAMETER_NOT_USED(storage_instance);
 UX_PARAMETER_NOT_USED(lun);
 UX_PARAMETER_NOT_USED(media_status);

 for (ULONG i = 0; i < number_blocks; i++)
 {
 fx_status = fx_media_read(&nor_flash_disk, lba + i, data_pointer + (i * SECTOR_SIZE_LOGICAL));

 if (fx_status != FX_SUCCESS)
 {
 status = UX_ERROR;
 break;
 }
 }
 /* USER CODE END USBD_STORAGE_Read */

 return status;
}

/**
 * @brief USBD_STORAGE_Write
 * This function is invoked to write in media.
 * @PAram storage_instance : Pointer to the storage class instance.
 * @PAram lun: Logical unit number is the command is directed to.
 * @PAram data_pointer: Address of the buffer to be used for reading or writing.
 * @PAram number_blocks: number of sectors to read/write.
 * @PAram lba: Logical block address is the sector address to read.
 * @PAram media_status: should be filled out exactly like the media status
 * callback return value.
 * @retval status
 */
UINT USBD_STORAGE_Write(VOID *storage_instance, ULONG lun, UCHAR *data_pointer,
 ULONG number_blocks, ULONG lba, ULONG *media_status)
{
 UINT status = UX_SUCCESS;

 /* USER CODE BEGIN USBD_STORAGE_Write */
 UINT fx_status;

 UX_PARAMETER_NOT_USED(storage_instance);
 UX_PARAMETER_NOT_USED(lun);
 UX_PARAMETER_NOT_USED(media_status);

 for (ULONG i = 0; i < number_blocks; i++)
 {
 fx_status = fx_media_write(&nor_flash_disk,
 lba + i,
 data_pointer + (i * SECTOR_SIZE_LOGICAL));

 if (fx_status != FX_SUCCESS)
 {
 status = UX_ERROR;
 break;
 }
 }
 /* USER CODE END USBD_STORAGE_Write */

 return status;
}

/**
 * @brief USBD_STORAGE_Flush
 * This function is invoked to flush media.
 * @PAram storage_instance : Pointer to the storage class instance.
 * @PAram lun: Logical unit number is the command is directed to.
 * @PAram number_blocks: number of sectors to read/write.
 * @PAram lba: Logical block address is the sector address to read.
 * @PAram media_status: should be filled out exactly like the media status
 * callback return value.
 * @retval status
 */
UINT USBD_STORAGE_Flush(VOID *storage_instance, ULONG lun, ULONG number_blocks,
 ULONG lba, ULONG *media_status)
{
 UINT status = UX_SUCCESS;

 /* USER CODE BEGIN USBD_STORAGE_Flush */
 UX_PARAMETER_NOT_USED(storage_instance);
 UX_PARAMETER_NOT_USED(lun);
 UX_PARAMETER_NOT_USED(number_blocks);
 UX_PARAMETER_NOT_USED(lba);
 UX_PARAMETER_NOT_USED(media_status);

 fx_media_flush(&nor_flash_disk);
 /* USER CODE END USBD_STORAGE_Flush */

 return status;
}

/**
 * @brief USBD_STORAGE_Status
 * This function is invoked to obtain the status of the device.
 * @PAram storage_instance : Pointer to the storage class instance.
 * @PAram lun: Logical unit number is the command is directed to.
 * @PAram media_id: is not currently used.
 * @PAram media_status: should be filled out exactly like the media status
 * callback return value.
 * @retval status
 */
UINT USBD_STORAGE_Status(VOID *storage_instance, ULONG lun, ULONG media_id,
 ULONG *media_status)
{
 UINT status = UX_SUCCESS;

 /* USER CODE BEGIN USBD_STORAGE_Status */
 UX_PARAMETER_NOT_USED(storage_instance);
 UX_PARAMETER_NOT_USED(lun);
 UX_PARAMETER_NOT_USED(media_id);

 *media_status = UX_SUCCESS;
 /* USER CODE END USBD_STORAGE_Status */

 return status;
}

/**
 * @brief USBD_STORAGE_Notification
 * This function is invoked to obtain the notification of the device.
 * @PAram storage_instance : Pointer to the storage class instance.
 * @PAram lun: Logical unit number is the command is directed to.
 * @PAram media_id: is not currently used.
 * @PAram notification_class: specifies the class of notification.
 * @PAram media_notification: response for the notification.
 * @PAram media_notification_length: length of the response buffer.
 * @retval status
 */
UINT USBD_STORAGE_Notification(VOID *storage_instance, ULONG lun, ULONG media_id,
 ULONG notification_class, UCHAR **media_notification,
 ULONG *media_notification_length)
{
 UINT status = UX_SUCCESS;

 /* USER CODE BEGIN USBD_STORAGE_Notification */
 UX_PARAMETER_NOT_USED(storage_instance);
 UX_PARAMETER_NOT_USED(lun);
 UX_PARAMETER_NOT_USED(media_id);
 UX_PARAMETER_NOT_USED(notification_class);
 UX_PARAMETER_NOT_USED(media_notification);
 UX_PARAMETER_NOT_USED(media_notification_length);
 /* USER CODE END USBD_STORAGE_Notification */

 return status;
}

/**
 * @brief USBD_STORAGE_GetMediaLastLba
 * Get Media last LBA.
 * @PAram none
 * @retval last lba
 */
ULONG USBD_STORAGE_GetMediaLastLba(VOID)
{
 ULONG LastLba = 0U;

 /* USER CODE BEGIN USBD_STORAGE_GetMediaLastLba */
 LastLba = TOTAL_SECTOR_LOGICAL - 1;
 /* USER CODE END USBD_STORAGE_GetMediaLastLba */

 return LastLba;
}

/**
 * @brief USBD_STORAGE_GetMediaBlocklength
 * Get Media block length.
 * @PAram none.
 * @retval block length.
 */
ULONG USBD_STORAGE_GetMediaBlocklength(VOID)
{
 ULONG MediaBlockLen = 0U;

 /* USER CODE BEGIN USBD_STORAGE_GetMediaBlocklength */
 MediaBlockLen = SECTOR_SIZE_LOGICAL;
 /* USER CODE END USBD_STORAGE_GetMediaBlocklength */

 return MediaBlockLen;
}


Windows see my disk but can't mount the volume : 

RemiNao_0-1759997613132.png

RemiNao_1-1759997625074.png

RemiNao_2-1759997679430.png

When windows see my USB Device, it wants to format it (but i use FileX to format it in my code, so windows don't see it i think) : 

RemiNao_3-1759997813467.png

RemiNao_4-1759997911495.png

And it says that windows cannot format the disk : 

RemiNao_5-1759997962740.png

 

Do you have any suggestions ?

 

3 replies

RemiNaoAuthor
Associate II
October 9, 2025

Windows only sees a USB drive and not a volume

MFARH.1
ST Employee
October 9, 2025

Hello @RemiNao ,

The USB device does not detect the media. Please ensure that your media is properly initialized and accessible before performing any read or write operations. Also, verify that the media initialization process completed without errors and that the storage device is properly connected and recognized by the system.

Regards,

Maher

RemiNaoAuthor
Associate II
October 9, 2025

Hello @MFARH.1 

Thank you for your reply,
I checked and tested the media initialization and I can't find any problems, there's just my media_memory variable where I'm not sure about its declaration. 

#define SECTOR_SIZE_LOGICAL 512 //512
#define TOTAL_SECTOR_LOGICAL 4096 // 4096

UCHAR media_memory[SECTOR_SIZE_LOGICAL];

 

UINT MX_FileX_Init(void)
{


 UINT ret = FX_SUCCESS;
 /* USER CODE BEGIN MX_FileX_Init */
 lx_stm32_nor_custom_driver_initialize(&nor_flash);

 /* USER CODE END MX_FileX_Init */

 /* Initialize FileX. */
 fx_system_initialize();

 /* USER CODE BEGIN MX_FileX_Init 1*/

 /* Format the NOR flash as FAT */
	 status = fx_media_format(&nor_flash_disk,
	 fx_stm32_levelx_nor_driver, // Driver entry
	 (VOID*)NOR_CUSTOM_DRIVER_ID, // Device info pointer
								(UCHAR*)media_memory, // Media buffer pointer
	 sizeof(media_memory), // Media buffer size
	 "NOR_FLASH_DISK", // Volume Name
	 1, // Number of FATs
	 32, // Directory Entries
	 0, // Hidden sectors
								TOTAL_SECTOR_LOGICAL,		 // Total sectors
								SECTOR_SIZE_LOGICAL, // Sector size
	 8, // Sectors per cluster
	 1, // Heads
	 1); // Sectors per track
 /* Check if the format status */
 if (status != FX_SUCCESS)
 {
 Error_Handler();
 }

 /* Open the SPI NOR Flash disk driver. */
 status = fx_media_open(&nor_flash_disk, "FX_LX_NOR_DISK", fx_stm32_levelx_nor_driver,(VOID*)NOR_CUSTOM_DRIVER_ID , media_memory, sizeof(media_memory));
 /* Check the media open status. */
 if (status != FX_SUCCESS)
 {
 Error_Handler();
 }

 /* Get the available usable space */
// status = fx_media_space_available(&nor_flash_disk, &available_space_pre);
// if (status != FX_SUCCESS)
// {
// Error_Handler();
// }
 /* USER CODE END MX_FileX_Init 1*/

 return ret;
}


Also, i tried this process and there is no errors : 

VOID MX_FileX_Process(void)
{
 UINT status;
 ULONG bytes_read;
 CHAR read_buffer[32];
 CHAR data[] = "This is FileX working on STM32";


/* Create a file called STM32.TXT in the root directory. */
 status = fx_file_create(&nor_flash_disk, "STM32.TXT");
 if (status != FX_SUCCESS)
 {
 if (status != FX_ALREADY_CREATED)
 Error_Handler();
 }

 /* Open the test file. */
 status = fx_file_open(&nor_flash_disk, &fx_file, "STM32.TXT", FX_OPEN_FOR_WRITE);
 if (status != FX_SUCCESS)
 Error_Handler();


 /* Seek to the beginning of the test file. */
 status = fx_file_seek(&fx_file, 0);
 if (status != FX_SUCCESS)
 Error_Handler();


 /* Write a string to the test file. */
 status = fx_file_write(&fx_file, data, sizeof(data));
 if (status != FX_SUCCESS)
 Error_Handler();


 /* Close the test file. */
 status = fx_file_close(&fx_file);
 if (status != FX_SUCCESS)
 Error_Handler();


 status = fx_media_flush(&nor_flash_disk);
 if (status != FX_SUCCESS)
 Error_Handler();


 /* Open the test file. */
 status = fx_file_open(&nor_flash_disk, &fx_file, "STM32.TXT", FX_OPEN_FOR_READ);
 if (status != FX_SUCCESS)
 Error_Handler();


 /* Seek to the beginning of the test file. */
 status = fx_file_seek(&fx_file, 0);
 if (status != FX_SUCCESS)
 Error_Handler();


 /* Read the first 28 bytes of the test file. */
 status = fx_file_read(&fx_file, read_buffer, sizeof(data), &bytes_read);
 if ((status != FX_SUCCESS) || (bytes_read != sizeof(data)))
 Error_Handler();


 /* Close the test file. */
 status = fx_file_close(&fx_file);
 if (status != FX_SUCCESS)
 Error_Handler();


 /* Close the media. */
// status = fx_media_close(&nor_flash_disk);
// if (status != FX_SUCCESS)
// Error_Handler();

}


Do you have any suggestions ?

 

MFARH.1
ST Employee
October 9, 2025

Hello @RemiNao,

Here is an example on the STM32H7 platform using the SD interface. You can refer to this project and replace the SD interface with your own custom interface as needed:
https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/STM32H735G-DK/Applications/USBX/Ux_Device_PIMA_MTP

 

Regards,

Maher