DCMIPP silient failure
- October 30, 2025
- 10 replies
- 502 views
Hello team,
Another day, new same issue. :pensive_face:
I have setup the DCMIPP PIPE 1 for the stm32n6570 DK, so that it dumps frames in address 0x34200000 which maps to SRAM3 begin address I have enabled bothe the memories SRAM3 and SRAM4 but with out software erase, I used the MX tool for project generation , I goal is to mimic the Continous Mode example provided by ST,
I have read about the appilication notes getting started with DCMIPP and the afew sections of intrest form the RM for the deve board on the topic.
I however face the challenge as stated in the Post Title, there Is are no interrups being called yet I set up the global intterrups for both the Pixel pipe and the CSI interfacing, "Still as shown in in the generated files" and set the clocks for the DCMIPP is set to 300Mhz and the CSI interface I had to manualy try setting up the input clock freq for the IMX335 module to 20Mz as the MX tool does not provide for its setting, but I have this code commented out as there was not change in the behavoir
I use the BSP bus pakage for the I2C communication, in outere to reduce the debug window,
My Question has any one knoledge about what could be going on wrongly, or what I have not done in order to have my setup running as expected, I have checked My project for any security blocks set up, by default, but none I have seen.
I noticed that the internal calls to the RCC may be ignored :crossed_fingers: as the IDE shows the intermost LL calls being greyed out. especially in the
#include "stm32n6xx_ll_bus.h" file

Find most of your querries in the attached files,