Skip to main content
Associate III
July 18, 2025
Question

Error using USB HS in STM32H747I-DISCO board

  • July 18, 2025
  • 1 reply
  • 317 views

Hello everyone,

I’ve recently acquired two STM32H747I-DISCO boards to experiment with USB High-Speed host functionality, specifically using the ux_host_hub_hid_msc example (v3.3.0) provided in the STM32CubeIDE.

My goal is to test the Mass Storage Class (MSC) capability, specifically writing a file to a USB flash drive. However, after flashing the example to either board, the USB device is not detected when I insert the pen drive, and LED7 on the DISCO board turns on immediately.

According to the reference manual, LED7 should light up green when the ULPI PHY detects a USB connection and the board is acting as a host. In my case, this LED turns on even before connecting any USB device.

massimoperdigo_1-1752837732433.png


Also, this function writes a pin that is not set in the FW (GPIO Pin 5 Port H):

/**
* @brief Drive VBUS.
* state : VBUS state
* This parameter can be one of the these values:
* 1 : VBUS Active
* 0 : VBUS Inactive
* @retval Status
*/
void USBH_DriverVBUS(uint8_t state)
{
 /* USER CODE BEGIN 0 */

 /* USER CODE END 0*/

 if (state == USB_VBUS_TRUE)
 {
 /* Drive high Charge pump */
 /* Add IOE driver control */
 /* USER CODE BEGIN DRIVE_HIGH_CHARGE_FOR_HS */
 HAL_GPIO_WritePin(GPIOH, GPIO_PIN_5, GPIO_PIN_SET);
 /* USER CODE END DRIVE_HIGH_CHARGE_FOR_HS */
 }
 else
 {
 /* Drive low Charge pump */
 /* Add IOE driver control */
 /* USER CODE BEGIN DRIVE_LOW_CHARGE_FOR_HS */
 HAL_GPIO_WritePin(GPIOH, GPIO_PIN_5, GPIO_PIN_RESET);
 /* USER CODE END DRIVE_LOW_CHARGE_FOR_HS */
 }

 HAL_Delay(200);
}

massimoperdigo_2-1752838349011.png

The USBH_DriverVBUS(USB_VBUS_TRUE) is called from the USBX_APP_Host_Init(VOID) function:

/**
 * @brief USBX_APP_Host_Init
 * Initialization of USB host.
 * none
 * @retval none
 */
VOID USBX_APP_Host_Init(VOID)
{
 /* USER CODE BEGIN USB_Host_Init_PreTreatment_0 */

 /* USER CODE END USB_Host_Init_PreTreatment_0 */

 /* Initialize the LL driver */
 MX_USB_OTG_HS_HCD_Init();

 /* Initialize the host controller driver */
 ux_host_stack_hcd_register(_ux_system_host_hcd_stm32_name,
 _ux_hcd_stm32_initialize, (ULONG)USB_OTG_HS,
 (ULONG)&hhcd_USB_OTG_HS);

 /* Drive vbus */
 USBH_DriverVBUS(USB_VBUS_TRUE);

 /* Enable USB Global Interrupt */
 HAL_HCD_Start(&hhcd_USB_OTG_HS);

 /* USER CODE BEGIN USB_Host_Init_PostTreatment1 */

 /* Start Application Message */
 USBH_UsrLog("**** USB OTG HS HUB HID MSC Host **** \n");
 USBH_UsrLog("USB Host library started.\n");

 /* Wait for Device to be attached */
 USBH_UsrLog("Starting HUB Application");
 USBH_UsrLog("Connect your HUB Device");

 /* USER CODE END USB_Host_Init_PreTreatment1 */
}

In fact, this pin corresponds to one input pins of the RAM memory:

massimoperdigo_3-1752838626566.png

screenshot from the design files MB1248-H747I-D03 (downloaded form ST)


Here’s my setup:

  • The board is powered via CN14 with 5V
  • JP6 is set to U5V to enable USB VBUS

Am I missing something in the setup? I was expecting LED7 to remain off until a USB mass storage device is actually connected.

Any suggestions or guidance would be greatly appreciated. Thanks in advance!

1 reply

Technical Moderator
August 21, 2025

Hi @massimoperdigo 

The example firmware is not working on your board? If so, provide the revision of the board? Is it MB1248-D04?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL