ETHERNET LWIP - STM32F429i - DP83848 Initialization Stuck / Clock Suspected Issue
Hi everyone,
I am working on a custom board based on the STM32F429I MCU (RMII mode) and I am trying to integrate LwIP with a DP83848 PHY.
At the moment, I am unable to get Ethernet working. The issue appears during PHY initialization — the code blocks while trying to communicate with the PHY over MDIO.
Project Context
MCU: STM32F429I
PHY: DP83848 (RMII mode)
Middleware: LwIP
Development tool: STM32CubeIDE (project originally generated with CubeMX, but I cannot re-generate it now due to version mismatch)
ETH driver: HAL
I have tried:
Using the LwIP stack with the HAL ETH driver
Attempting raw Ethernet (without LwIP)
In both cases, the system gets stuck during PHY initialization.
Observed Behavior
The code freezes when accessing PHY registers (MDIO communication).
When debugging, execution appears to stop when checking or configuring the ETH clock.
The PHY does not respond to register reads.
Suspected Cause
I suspect either:
The RMII clock (50 MHz reference clock) is not correctly generated or routed.
The PHY hardware wiring may be incorrect.
MDIO/MDC lines may not be functioning properly.
Since the failure occurs during clock/PHY access, I am leaning toward a hardware or clock configuration issue rather than a pure LwIP software problem.
Questions
Has anyone successfully integrated STM32F429I + DP83848 in RMII mode with LwIP?
Are there known pitfalls regarding:
RMII clock source configuration (MCO vs external oscillator)?
PHY address configuration?
Required CubeMX ETH clock settings?
Is there a recommended minimal test (without LwIP) to validate only MAC ↔ PHY communication?
Additional Information
If needed, I can provide:
ETH clock configuration
Schematic excerpt (RMII + PHY section)
PHY address and strap configuration
Debug register values
Any guidance on how to isolate whether this is a hardware or software issue would be greatly appreciated.
Thank you in advance.