Skip to main content
Associate
August 21, 2025
Question

H7S3L8 with ethernet and Lwip is creating hardfault

  • August 21, 2025
  • 1 reply
  • 403 views



I have followed the article (https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308#memory-layout ) to get it working for ethernet but I am facing hardfault. In H7S3L8 I am using AXI-SRAM at address 0x24020000 for ethernet buffers and lwip and configuring this sram as non cacheable, non bufferable and shareable at level 1 


I am getting hardfault. I is related to memory but I am not able to resolve it. Any help me to find where is the  problem?

imranhassan84_2-1755796501200.png

 



imranhassan84_0-1755795691511.png



imranhassan84_1-1755796411796.png

 




Linker file is shown below

 

/*

******************************************************************************

**

** @file : LinkerScript.ld

**

** @author : STM32CubeIDE

**

** Abstract : Linker script for STM32H7Sxx Device

** 64Kbytes FLASH

** 456Kbytes RAM

**

** Set heap size, stack size and stack location according

** to application requirements.

**

** Set memory bank area and size if external memory is used

**

** Target : STMicroelectronics STM32

**

** Distribution: The file is distributed as is, without any warranty

** of any kind.

**

******************************************************************************

** @attention

**

** Copyright (c) 2025 STMicroelectronics.

** All rights reserved.

**

** This software is licensed under terms that can be found in the LICENSE file

** in the root directory of this software component.

** If no LICENSE file comes with this software, it is provided AS-IS.

**

******************************************************************************

*/



/* Entry Point */

ENTRY(Reset_Handler)



/* Highest address of the user mode stack */

_estack = ORIGIN(DTCM) + LENGTH(DTCM); /* end of Ram type memory */



_Min_Heap_Size = 0x200; /* required amount of heap */

_Min_Stack_Size = 0x400; /* required amount of stack */



/*__FLASH_BEGIN = 0x08000000;*/

/*__FLASH_SIZE = 0x00010000;*/





__FLASH_BEGIN = 0x00000000;

__FLASH_SIZE = 0x00030000;





__RAM_BEGIN = 0x24000000;

__RAM_SIZE = 0x71C00;

__RAM_NONCACHEABLEBUFFER_SIZE = 0x400;



/* Memories definition */

MEMORY

{

RAM (xrw) : ORIGIN = __RAM_BEGIN, LENGTH = __RAM_SIZE

RAM_NONCACHEABLEBUFFER (xrw) : ORIGIN = __RAM_BEGIN + __RAM_SIZE, LENGTH = __RAM_NONCACHEABLEBUFFER_SIZE



ITCM (xrw) : ORIGIN = 0x00000000, LENGTH = 0x00030000

DTCM (rw) : ORIGIN = 0x20000000, LENGTH = 0x00030000

SRAMAHB (rw) : ORIGIN = 0x30000000, LENGTH = 0x00008000

BKPSRAM (rw) : ORIGIN = 0x38800000, LENGTH = 0x00001000

SRAMAXI (rw) : ORIGIN = 0x24020000, LENGTH = 0x00020000



FLASH (xrw) : ORIGIN = __FLASH_BEGIN, LENGTH = __FLASH_SIZE

}



/* Sections */

SECTIONS

{

/* The startup code into "FLASH" Rom type memory */

.isr_vector :

{

. = ALIGN(4);

KEEP(*(.isr_vector)) /* Startup code */

. = ALIGN(4);

} >FLASH



.lwip_sec (NOLOAD):

{

. = ABSOLUTE(0x24020000);

*(.RxDescripSection)



. = ABSOLUTE(0x24020080);

*(.TxDescripSection)



. = ABSOLUTE(0x24020100);

*(.Rx_PoolSection)





} >SRAMAXI





.hf_debug (NOLOAD) : { *(.hf_debug*) } > DTCM



/* The program code and other data into "FLASH" Rom type memory */

.text :

{

. = ALIGN(4);

*(.text) /* .text sections (code) */

*(.text*) /* .text* sections (code) */

*(.glue_7) /* glue arm to thumb code */

*(.glue_7t) /* glue thumb to arm code */

*(.eh_frame)



KEEP (*(.init))

KEEP (*(.fini))



. = ALIGN(4);

_etext = .; /* define a global symbols at end of code */

} >FLASH



/* Constant data into "FLASH" Rom type memory */

.rodata :

{

. = ALIGN(4);

*(.rodata) /* .rodata sections (constants, strings, etc.) */

*(.rodata*) /* .rodata* sections (constants, strings, etc.) */

. = ALIGN(4);

} >FLASH



.ARM.extab (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */

{

. = ALIGN(4);

*(.ARM.extab* .gnu.linkonce.armextab.*)

. = ALIGN(4);

} >FLASH

.ARM (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */

{

. = ALIGN(4);

__exidx_start = .;

*(.ARM.exidx*)

__exidx_end = .;

. = ALIGN(4);

} >FLASH



.preinit_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */

{

. = ALIGN(4);

PROVIDE_HIDDEN (__preinit_array_start = .);

KEEP (*(.preinit_array*))

PROVIDE_HIDDEN (__preinit_array_end = .);

. = ALIGN(4);

} >FLASH



.init_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */

{

. = ALIGN(4);

PROVIDE_HIDDEN (__init_array_start = .);

KEEP (*(SORT(.init_array.*)))

KEEP (*(.init_array*))

PROVIDE_HIDDEN (__init_array_end = .);

. = ALIGN(4);

} >FLASH



.fini_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */

{

. = ALIGN(4);

PROVIDE_HIDDEN (__fini_array_start = .);

KEEP (*(SORT(.fini_array.*)))

KEEP (*(.fini_array*))

PROVIDE_HIDDEN (__fini_array_end = .);

. = ALIGN(4);

} >FLASH



/* Used by the startup to initialize data */

_sidata = LOADADDR(.data);



/* Initialized data sections into "RAM" Ram type memory */

.data :

{

. = ALIGN(4);

_sdata = .; /* create a global symbol at data start */

*(.data) /* .data sections */

*(.data*) /* .data* sections */

*(.RamFunc) /* .RamFunc sections */

*(.RamFunc*) /* .RamFunc* sections */



. = ALIGN(4);

_edata = .; /* define a global symbol at data end */



} >RAM AT> FLASH



/* Uninitialized data section into "RAM" Ram type memory */

. = ALIGN(4);

.bss :

{

/* This is used by the startup in order to initialize the .bss section */

_sbss = .; /* define a global symbol at bss start */

__bss_start__ = _sbss;

*(.bss)

*(.bss*)

*(COMMON)



. = ALIGN(4);

_ebss = .; /* define a global symbol at bss end */

__bss_end__ = _ebss;

} >RAM



RW_NONCACHEABLE :

{

__NONCACHEABLEBUFFER_BEGIN = .;/* create symbol for start of section */

KEEP(*(noncacheable_buffer))

__NONCACHEABLEBUFFER_END = .; /* create symbol for start of section */

} > RAM_NONCACHEABLEBUFFER



/* User_heap_stack section, used to check that there is enough Ram type memory left */

._user_heap_stack :

{

. = ALIGN(8);

PROVIDE ( end = . );

PROVIDE ( _end = . );

. = . + _Min_Heap_Size;

. = . + _Min_Stack_Size;

. = ALIGN(8);

} >DTCM



/* Remove information from the compiler libraries */

/DISCARD/ :

{

libc.a ( * )

libm.a ( * )

libgcc.a ( * )

}



.ARM.attributes 0 : { *(.ARM.attributes) }

}

 

 

1 reply

Technical Moderator
August 22, 2025

Hello @imranhassan84, and welcome to ST community!

I suggest you take a look at the following LwIP projects for the H7S3L8. You can draw inspiration from them and adapt them to suit your application needs. Additionally, each project includes the appropriate IOC configuration file, which you can review and modify.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.