HAL_NVIC_SystemReset() don't work on STM32H755
hello ST Community,
I'm developing the bootloader for the STM32H755 microcontroller from a specific flash memory address of 0x08010000. I also modified the USER_VECT_TAB_ADDRESS definition in the file 'system_stm32h7xx_dualcore_boot_cm4_cm7.c', as follows:
/************************* Miscellaneous Configuration ************************/
/* Note: Following vector table addresses must be defined in line with linker
configuration. */
/*!< Uncomment the following line if you need to relocate the vector table
anywhere in FLASH BANK1 or AXI SRAM, else the vector table is kept at the automatic
remap of boot address selected */
#define USER_VECT_TAB_ADDRESS
#define FLASH_BANK1_BASE 0x08010000U
#if defined(USER_VECT_TAB_ADDRESS)
#if defined(CORE_CM4)
/*!< Uncomment the following line if you need to relocate your vector Table
in D2 AXI SRAM else user remap will be done in FLASH BANK2. */
/* #define VECT_TAB_SRAM */
#if defined(VECT_TAB_SRAM)
#define VECT_TAB_BASE_ADDRESS D2_AXISRAM_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x400. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x400. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BANK2_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x400. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x400. */
#endif /* VECT_TAB_SRAM */
#elif defined(CORE_CM7)
/*!< Uncomment the following line if you need to relocate your vector Table
in D1 AXI SRAM else user remap will be done in FLASH BANK1. */
/* #define VECT_TAB_SRAM */
#if defined(VECT_TAB_SRAM)
#define VECT_TAB_BASE_ADDRESS D1_AXISRAM_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x400. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x400. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BANK1_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x400. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x400. */
#endif /* VECT_TAB_SRAM */
#else
#error Please #define CORE_CM4 or CORE_CM7
#endif /* CORE_CM4 */
#endif /* USER_VECT_TAB_ADDRESS */
/******************************************************************************/
When the software starts, it starts correctly from address 0x08010000, as per the following build analyzer analysis.

But when I press reset and then call the function HAL_NVIC_SystemReset(), it doesn't restart. I'm afraid it won't restart from address 0x08010000, I'm afraid I've incorrectly defined USER_VECT_TAB_ADDRESS. What's wrong and what else is missing to make resetting and rebooting from work correctly?
thanks for supports