Impact of changing ThreadX timebase to 1ms
I have changed the ThreadX system timebase on an STM32H7 from 10 ms to 1 ms (i.e., the RTOS tick is now 1 ms). The application is quite large and makes extensive use of ThreadX services such as thread delays, semaphores, mutexes, event flags, and timeouts in various system calls, all of which are specified in ticks. With this change, the real-time duration of existing delays and timeouts is effectively reduced (for example, a delay that was previously 1 second now becomes 100 ms), so I would like to understand whether these values need to be scaled accordingly or refactored using time-based conversion macros to preserve behavior. In addition, the system uses NetX Duo, which runs on top of ThreadX, and I would like to confirm whether NetX Duo fully depends on the same ThreadX tick and whether changing the tick period to 1 ms has implications for network timing, such as TCP timeouts, retransmissions, or protocol timers. Finally, I am interested in best practices and potential risks, such as increased CPU load, timing jitter, or stability issues, when moving to a 1 ms tick on STM32H7, and how to adjust the system safely so the application continues to run reliably without crashes.