Is X-CUBE-AUDIO-KIT Livetune compatible with both versions of STM32H573I-DK?
Hi all,
I'm planning to get STM32H573I-DK to evaluate X-CUBE-AUDIO-KIT Livetune because there are project examples for specific boards and this is one of them. I'll be using an STM32U5A9 MCU eventually and both have an M33 core. This should make it easier to port from one to the other. I see that there are two versions of STM32H573I-DK:

MB1677-H573I-D01 Board schematic has a WM8904 audio codec and MB1677-H573I-C02 Board schematic has a CS42L51 audio codec. This last one is marked as "Discontinued Product" by the manufacturer.
Do the examples for STM32H573I-DK work for either version of the board without any modification or does it require a specific version/codec?
Thanks.