Issue Using Internal 4.2MB SRAM (0x34000000) as LTDC Framebuffer – RGB Signals Inactive
- February 14, 2026
- 1 reply
- 311 views
Dear ST Support Team,
I am currently working with the STM32N657X0H3 microcontroller.
We are attempting to use the internal 4.2 MB continuous SRAM (starting at address 0x34000000) as the framebuffer for LTDC.
The procedure followed is:
• Writing pixel data into internal SRAM at 0x34000000
• Configuring LTDC_Layer1->CFBAR with the same framebuffer address
• Enabling LTDC and RGB output
However, when using the internal SRAM (0x34000000) as the framebuffer, the RGB output signals remain inactive.
When we configure the framebuffer in DTCM memory (as mentioned in the reference manual), the RGB signals become active and function as expected.
However, the DTCM memory size is very small and not sufficient to hold a full framebuffer for our display resolution. Therefore, using DTCM is not a practical solution for our application.
We have verified the following:
• AXI read/write test passes successfully
• Framebuffer base address is correctly configured
• LTDC timing configuration is correct
• RGB pin configuration is verified
• No bus faults are observed
We would like guidance on the following:
How should the internal 4.2 MB continuous SRAM be configured to be accessible by LTDC?
What MPU attributes (cacheable, bufferable, shareable) are recommended for LTDC framebuffer memory?
Are there any AXI/AHB bus matrix or domain clock requirements for LTDC access to this SRAM region?
Are there any restrictions preventing LTDC from accessing 0x34000000?
We have attached the relevant initialization code and configuration files for your reference.
Kindly provide your guidance on how to correctly configure the internal SRAM to enable active RGB signals.
Best regards,
Shivani Elavena