Skip to main content
JacquiG29
Associate
February 6, 2026
Question

line-in data clipped in STM32H735G-DK

  • February 6, 2026
  • 3 replies
  • 188 views

I am trying to capture data from the LINE_IN (blue jack on board), but I am not receiving the correct input. I evaluated my output at the oscilloscope and noticed that I am not receiving the sinusoid I am injecting; the frequency is correct, but the data appears clipped, as shown in the picture. I tried to reduce the Vpp, but it just started getting noisy instead of giving the correct input.

wave.jpeg

My second test was to record on the sd card, and the problem persisted; I am only getting data above zero and noise

Figure_1.png

I am using the BSP library stm32h735g_discovery_audio.c, and to get the correct frequency that I was inputting, I modified these values in the BSP_AUDIO_IN_Init

mx_config.FrameLength = 64;//changed: prev:128
mx_config.ActiveFrameLength = 32;//changed /

An changed the number of slots like this:

hsai->SlotInit.SlotNumber = 4; /* WM8994 TDM mode: 4 slots */

I also tried to modify these registers from the audio codec directly, but nothing seems to make it work:

* Disable mute on IN1L_TO_MIXINL and +30dB on IN1L PGA output */
//tmp = 0x0035;
//ret += wm8994_write_reg(&pObj->Ctx, WM8994_INPUT_MIXER_3, &tmp, 2);
/* CHANGE! MIXOUTR_MIXINR_VOL set to 0 (mute)
* +30db removed : 0x0020 instead of 0x0035 */
tmp = 0x0020;
ret += wm8994_write_reg(&pObj->Ctx, WM8994_INPUT_MIXER_3, &tmp, 2);

/* Disable mute on IN1R_TO_MIXINL, Gain = +30dB */
//ret += wm8994_write_reg(&pObj->Ctx, WM8994_INPUT_MIXER_4, &tmp, 2);
/* CHANGE! MIXOUTL_MIXINL_VOL set to 0 (mute)
* +30db removed : 0x0020 instead of 0x0035 */
tmp = 0x0020;
ret += wm8994_write_reg(&pObj->Ctx, WM8994_INPUT_MIXER_4, &tmp, 2);: 

/* Enable VMID and Master Bias - Critical for LINE_IN to capture negative cycle */
tmp = 0x0007;
ret += wm8994_write_reg(&pObj->Ctx, WM8994_PWR_MANAGEMENT_1, &tmp, 2);

Does anyone have experienced the same issue and have suggestions on how to solve this problem? This is how I am initializing the input and output.

int Audio_LoopbackInit(void)
{
 BSP_AUDIO_Init_t AudioInInit;
 BSP_AUDIO_Init_t AudioOutInit;

 /* Configure audio INPUT (LINE_IN) */
 AudioInInit.Device = AUDIO_IN_DEVICE_ANALOG_LINE1; /* LINE_IN jack */
 AudioInInit.ChannelsNbr = 2; /* Stereo */
 AudioInInit.SampleRate = AUDIO_FREQUENCY_48K;
 AudioInInit.BitsPerSample = AUDIO_RESOLUTION_16B;
 AudioInInit.Volume = 100;

 /* Instance 0 = SAI/LINE_IN (NOT Instance 2 which is DFSDM/digital mics) */
 if (BSP_AUDIO_IN_Init(0, &AudioInInit) != BSP_ERROR_NONE)
 {
 return -1; /* Failed - check codec I2C connection */
 }

 /* Configure audio OUTPUT (Headphone) */
 AudioOutInit.Device = AUDIO_OUT_DEVICE_HEADPHONE;
 AudioOutInit.ChannelsNbr = 2;
 AudioOutInit.SampleRate = AUDIO_FREQUENCY_48K;
 AudioOutInit.BitsPerSample = AUDIO_RESOLUTION_16B;
 AudioOutInit.Volume = 50;

 if (BSP_AUDIO_OUT_Init(0, &AudioOutInit) != BSP_ERROR_NONE)
 {
 return -2; /* Failed */
 }

 return 0;
}

EDIT: The problem was this function, I needed to configure the BSP_AUDIO_OUT_Init first

3 replies

Technical Moderator
February 25, 2026

Hello @JacquiG29 

I suspect SAI Codec initialization issue or data format misconfiguration. An internal ticket is submitted to dedicated team for further investigation (227889).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
T_Hamdi
ST Employee
April 7, 2026

Hello  

Could you please give me more details about your application, including your starting point, and share it with me if possible so that I can help resolve the issue? 

Best regards

Hamdi

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Hamdi Teyeb"
Technical Moderator
April 22, 2026

Hello @JacquiG29 

It seems you find out the root cause of the issue : the initialization order of the audio codec paths. On this board, the playback and capture paths share codec resources, so it is important to initialize the output path first:

int Audio_LoopbackInit(void)
{
 BSP_AUDIO_Init_t AudioInInit;
 BSP_AUDIO_Init_t AudioOutInit;
 AudioOutInit.Device = AUDIO_OUT_DEVICE_HEADPHONE;
 AudioOutInit.ChannelsNbr = 2;
 AudioOutInit.SampleRate = AUDIO_FREQUENCY_48K;
 AudioOutInit.BitsPerSample = AUDIO_RESOLUTION_16B;
 AudioOutInit.Volume = 50;
 if (BSP_AUDIO_OUT_Init(0, &AudioOutInit) != BSP_ERROR_NONE)
 {
 return -2;
 }
 AudioInInit.Device = AUDIO_IN_DEVICE_ANALOG_LINE1;
 AudioInInit.ChannelsNbr = 2;
 AudioInInit.SampleRate = AUDIO_FREQUENCY_48K;
 AudioInInit.BitsPerSample = AUDIO_RESOLUTION_16B;
 AudioInInit.Volume = 100;
 if (BSP_AUDIO_IN_Init(0, &AudioInInit) != BSP_ERROR_NONE)
 {
 return -1;
 }
 return 0;
}

Could you please confirm whether the issue is now resolved on your side?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL