Skip to main content
Associate II
September 8, 2024
Question

Problem with HAL_ADC_PollForConversion() when debugging.

  • September 8, 2024
  • 1 reply
  • 1073 views

Hi everybody,

I'm learning to use the ADC in a STM32F411CEU in Continuous Mode and Single Conversion with Polling. When the code is downloaded to the MCU everything runs ok (I mean, when the MCU runs by itself without any ST-Link connected).

The problem appears when I try to execute the code in a debugging session. The first time the function HAL_ADC_PollForConversion() is called, the result is HAL_OK, but in the next iterations the functions doesn't return HAL_OK anymore.

I know, I know, with Continuous Mode I should be using DMA. But I'm trying to learn the different operation modes (single conversion, scan mode, polling, DMA, etc.)

One thing I've found is that if I set the ADC parameter

 

End Of Conversion Selection = EOC flag at the end of all conversions

 

instead of

 

End Of Conversion Selection = EOC flag at the end of single channel conversion

 

, then the function HAL_ADC_PollForConversion() works ok in all the iterations when debugging.

 

Can anybody explain me what am I doing wrong?

Thanks in advance.

 

This is the code:

 

 

do { status_adc = HAL_ADC_Start(&hadc1); } while (status_adc != HAL_OK);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
 {
while (HAL_ADC_PollForConversion(&hadc1, 10) != HAL_OK) {}
 input = HAL_ADC_GetValue(&hadc1);

 

1 reply

SPere.5
Visitor II
March 4, 2026

Exactly same issue in STM32F429. 

I monitor ADC flags EOC is set and after a few cycles it is going back to 0. 

HAL Polling function stays polling for this flag but it never get it at 1. This is why it gives HAL_TIMEOUT.

Moving to 

End Of Conversion Selection = EOC flag at the end of all conversions

fixed the issue. I don't understand how in this mode EOC is kept 1 permanently. 

Very weird behaviour even if using 1 channel conversion setting EOC to single conversion mode when trying to enable continuous conversions breaks the ADC lecture. 

ST should fix this.