Skip to main content
Associate III
July 8, 2025
Question

Re: Setup USB-OTG-FS with Mass Storage Class on a STM32469 Discovery Board with CubeMX

  • July 8, 2025
  • 1 reply
  • 250 views

hey @m.beddi , 
have you find the solution . i am struck at this too.

edit : to reformulate the issue

Issue description :

I am trying to implement the MSC_Standalone example (USB device mode with SD card) on the STM32469 Discovery board using CubeMX (with USB OTG FS mode).

  • USB initialization appears to work, but the SD card is not recognized or accessible.
  • The program hangs with a timeout error in the SD card command response function SDMMC_GetCmdResp1(), indicating that SD card commands are not completing successfully.
  • I suspect a timing or clock configuration issue, despite trusting CubeMX to handle this.
uint32_t SDMMC_GetCmdResp1(SDIO_TypeDef *SDIOx, uint8_t SD_CMD, uint32_t Timeout)
{
 uint32_t response_r1;
 uint32_t sta_reg;
 uint32_t count = Timeout * (SystemCoreClock / 8U / 1000U);
 do
 {
 if (count-- == 0U)
 {
 return SDMMC_ERROR_TIMEOUT;
 }
 sta_reg = SDIOx->STA;
 } while (((sta_reg & (SDIO_FLAG_CCRCFAIL | SDIO_FLAG_CMDREND | SDIO_FLAG_CTIMEOUT)) == 0U) ||
 ((sta_reg & SDIO_FLAG_CMDACT) != 0U));
}

 

I would appreciate any advice or best practices on how to troubleshoot and resolve this issue, especially regarding clock configuration, SD card initialization, or CubeMX project setup. The complexity of clock and peripheral setup is overwhelming, so any guidance would be very helpful.

1 reply

Technical Moderator
August 6, 2025

Hi @Prajyot1 

Did you test the SD card with another device? Ensure it is formatted with a supported file system (usually FAT32) and is not corrupted. Otherwise the example itself should be working without issues.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL