Skip to main content
Explorer
March 10, 2026
Question

RTC SSR Underflow Interrupt on H533 ? (Low Layer Drivers)

  • March 10, 2026
  • 3 replies
  • 208 views

I'm failing to enable that Interrupt using " LL_RTC_EnableIT_SSRU(RTC) " on STM32H33.

Wakeup timer is set to interrupt every 24h (this is working).

Alarm A is configured, but not enabled.

Alarm B is not used.

RTC is set to BCD mode only.

Monitoring SSR register ( via "READ_REG(RTC->SSR)" ) I can see it's counting down from 0xFF ---> 0x00, periodically.

Some Internet folks told me to enable TAMP Interrupt as well...and intercept TAMP IRQ handler instaead of RTC IRQ handler. It didn't work.

Any help would be greatly appreciated.

Thanks.

 

 

 

 

3 replies

Chris21
Associate II
March 10, 2026

I noticed this comment in the HAL header file:

/**
* @brief Enable SSR Underflow interrupt
* @note Bit is write-protected. @ref LL_RTC_DisableWriteProtection function should be called before.
* @rmtoll RTC_CR SSRUIE LL_RTC_EnableIT_SSRU
* @PAram RTCx RTC Instance
* @retval None
*/

Technical Moderator
March 16, 2026

Hello @peplegal 
the bit is write-protected.
Can you try and call LL_RTC_DisableWriteProtection before calling LL_RTC_EnableIT_SSRU adn see if it solves your problem.
BR
Gyessine

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Technical Moderator
April 3, 2026

Hello @peplegal 
Any updates, did you solve your problem?
BR
Gyessine

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.