RTOS debugging with CubeIDE
Hi everyone
I've got a few questions about the views that show FreeRTOS Semaphores and Queues:
1. My application creates a lot of Mutex and Queues, and only the first 63 (or 64 -- I may have lost count) of each type are visible. Is this a feature or a bug? And if I want to see the remainder... any thoughts on how to go about that?
2. Here's a screenshot of the Semaphore view:
2A: MutexSPI2 is created by CubeMX as a dynamically allocated Mutex using the CMSIS OS wrapper.
2B: PS-Global Lock is created with
mutex_init(&lock,"PS-Global Lock");where
int mutex_init(mutex_t *_m, const char* mutex_name) {
SemaphoreHandle_t *m = (SemaphoreHandle_t *) _m;
*m = xSemaphoreCreateMutex();
vQueueAddToRegistry((QueueHandle_t) m,mutex_name);
return 0;
}I'm guessing that since the 'mutex' is being defined as a Semaphore is why it's not showing up on the list as a MUTEX, but I don't understand why the "Size" and "Free" values are.
2C: The remainder of the Semaphores are created by
ps_queue_t *q = calloc(1, sizeof(ps_queue_t));
mutex_init(&q->mux, mutex_name);
semaphore_init(&q->not_empty, 0, sem_name);where
int semaphore_init(semaphore_t *_s, unsigned int value, const char* sem_name) {
SemaphoreHandle_t *s = (SemaphoreHandle_t *) _s;
*s = xSemaphoreCreateCounting(INT32_MAX, value);
vQueueAddToRegistry((QueueHandle_t) s,sem_name);
return 0;
}I don't understand why the Free and # Blocked Tasks values are so large (other than they look like
pointers to code addresses).
The code does work (I'm using the pubsub-c library from here
https://github.com/jaracil/pubsub-c and modified it so each mutex / semaphore gets assigned
a name so I could tell them apart.
I'm trying to understand what the values mean and if they're important for what I'm using.
Yes, I should probably spend some time reading through the library but was hoping someone could
tell me if it's a feature or a bug...
I suppose the biggest question is how this view gets the info it's looking for, and if I'm
mis-interpreting the lists because it's a mutex being viewed as a semaphore, or vice versa.
Hope this makes sense to someone other than me, and thank you for your time