SD CARD reading issue using STM32H723ZGT6 Nucleo board
Hai Everyone,
I am currently working with the STM32H723ZGT6 Nucleo board to implement basic SD card read and write functionality.
I have enabled RCC, configured HSE and PLL, and set the system clock to 240 MHz. The SDMMC kernel clock is sourced from PLL1Q at 48 MHz.
I tested the SD interface in both 1-bit mode and 4-bit wide bus mode. While the write operation is working correctly, I am unable to read data from the SD card.
I would appreciate it if someone could help me resolve this issue. Your support would be very helpful.
Thankyou.
Best Regards,
Aashritha