Skip to main content
Associate III
August 10, 2025
Solved

Standalone FileX SDIO SD Card Initializing errors

  • August 10, 2025
  • 1 reply
  • 596 views

Hello Community,

I am trying to initialize SD card with FileX middleware standalone with my Nucleo-U545RET6Q board.

I have initialized SDMMC1 with SD 4 bit wide , 48MHz with 0 divider. Later i had to put divider by 2 because the code was stuck at fx_media_open(); here is the picture:

frogrammer_0-1754826108415.png

 

Later I have initialized the FileX middleware with SD interface, without changing any parameters. I then, edited the app_filex.c using code found with RTOS Based SD File edit program in U5 families. 

This is my app_filex.c file

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file app_filex.c
 * @author MCD Application Team
 * @brief FileX applicative file
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2021 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "app_filex.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "main.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define FX_STM32_SD_DEFAULT_SECTOR_SIZE 4096
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */
/* Define FileX global data structures. */
/* FileX SRAM disk media instance */
FX_MEDIA sdio_disk;
/* FileX file instance */
FX_FILE fx_file;

ALIGN_32BYTES (uint32_t fx_sd_media_memory[FX_STM32_SD_DEFAULT_SECTOR_SIZE / sizeof(uint32_t)]);

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/

/* USER CODE BEGIN PFP */

/* USER CODE END PFP */
/**
 * @brief Application FileX Initialization.
 * None
 * @retval int
 */
UINT MX_FileX_Init(void)
{
 UINT ret = FX_SUCCESS;
 /* USER CODE BEGIN MX_FileX_Init */

 /* USER CODE END MX_FileX_Init */

 /* Initialize FileX. */
 fx_system_initialize();

 /* USER CODE BEGIN MX_FileX_Init 1*/

 /* USER CODE END MX_FileX_Init 1*/

 return ret;
}

/* USER CODE BEGIN 1 */
VOID MX_FileX_Process(void)
{
 UINT status;
 ULONG bytes_read;
 CHAR read_buffer[32];
 CHAR data[] = "This is FileX working on STM32";

 /* Start application */
 printf("FileX SD Standalone Application Start.\n");

 /* Open the sd_disk driver. */
 status = fx_media_open(&sdio_disk, "STM32_SD_DISK", fx_stm32_sd_driver, (VOID *)FX_NULL, (VOID *) fx_sd_media_memory, sizeof(fx_sd_media_memory));

 /* Check the media open status. */
 if (status != FX_SUCCESS)
 {
 Error_Handler();
 }

 printf("SD Disk successfully opened.\n");

 /* Create a file called STM32.TXT in the root directory. */
 status = fx_file_create(&sdio_disk, "STM33.TXT");

 /* Check the create status. */
 if (status != FX_SUCCESS)
 {
 /* Check for an already created status. This is expected on the
 second pass of this loop! */
 if (status != FX_ALREADY_CREATED)
 {
 /* Create error, call error handler. */
 Error_Handler();
 }
 }

 /* Open the test file. */
 status = fx_file_open(&sdio_disk, &fx_file, "STM33.TXT", FX_OPEN_FOR_WRITE);

 /* Check the file open status. */
 if (status != FX_SUCCESS)
 {
 /* Error opening file, call error handler. */
 Error_Handler();
 }

 /* Seek to the beginning of the test file. */
 status = fx_file_seek(&fx_file, 0);

 /* Check the file seek status. */
 if (status != FX_SUCCESS)
 {
 /* Error performing file seek, call error handler. */
 Error_Handler();
 }

 printf("Writing data into the file. \n");

 /* Write a string to the test file. */
 status = fx_file_write(&fx_file, data, sizeof(data));

 /* Check the file write status. */
 if (status != FX_SUCCESS)
 {
 /* Error writing to a file, call error handler. */
 Error_Handler();
 }

 /* Close the test file. */
 status = fx_file_close(&fx_file);

 /* Check the file close status. */
 if (status != FX_SUCCESS)
 {
 /* Error closing the file, call error handler. */
 Error_Handler();
 }

 status = fx_media_flush(&sdio_disk);

 /* Check the media flush status. */
 if (status != FX_SUCCESS)
 {
 /* Error closing the file, call error handler. */
 Error_Handler();
 }

 /* Open the test file. */
 status = fx_file_open(&sdio_disk, &fx_file, "STM33.TXT", FX_OPEN_FOR_READ);

 /* Check the file open status. */
 if (status != FX_SUCCESS)
 {
 /* Error opening file, call error handler. */
 Error_Handler();
 }

 /* Seek to the beginning of the test file. */
 status = fx_file_seek(&fx_file, 0);

 /* Check the file seek status. */
 if (status != FX_SUCCESS)
 {
 /* Error performing file seek, call error handler. */
 Error_Handler();
 }

 /* Read the first 28 bytes of the test file. */
 status = fx_file_read(&fx_file, read_buffer, sizeof(data), &bytes_read);

 /* Check the file read status. */
 if ((status != FX_SUCCESS) || (bytes_read != sizeof(data)))
 {
 /* Error reading file, call error handler. */
 Error_Handler();
 }

 /* Close the test file. */
 status = fx_file_close(&fx_file);

 /* Check the file close status. */
 if (status != FX_SUCCESS)
 {
 /* Error closing the file, call error handler. */
 Error_Handler();
 }

 /* Close the media. */
 status = fx_media_close(&sdio_disk);

 /* Check the media close status. */
 if (status != FX_SUCCESS)
 {
 /* Error closing the media, call error handler. */
 Error_Handler();
 }

 printf("Data successfully written.\n");

 /* Infinite loop */
 while (1)
 {
 HAL_GPIO_TogglePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin);
 HAL_Delay(500);
 }
}
/* USER CODE END 1 */

 

Note that default  #define FX_STM32_SD_DEFAULT_SECTOR_SIZE 512  doesn't work until i make it 2*512 in my program, later i make it 4096.  

My program runs until i go to :

 status = fx_media_flush(&sdio_disk);

 /* Check the media flush status. */
 if (status != FX_SUCCESS)
 {
 /* Error closing the file, call error handler. */
 Error_Handler();
 }

 

Here the Errror_Handler(); is invoked, and from the debugger i get these statues with status code = 144,

frogrammer_1-1754826904174.png

 

There was once it could successfully write the text file onto the sd card 

frogrammer_2-1754827007817.png

but again that was once and even that time the fx_media_flush() error occurred. 

 

I wanted to know how can i get around this error, and reliably read write delete files into sd card for a datalogger project.

Best answer by Saket_Om

Hello @frogrammer 

Mybe it is better to try it on this example below:

STM32CubeU5/Projects/STM32U575I-EV/Applications/FileX/Fx_File_Edit_Standalone at main · STMicroelectronics/STM32CubeU5 · GitHub

1 reply

Technical Moderator
August 13, 2025

Hello @frogrammer 

What is the sector size of your SD card? Please check the datasheet of your device. 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Associate III
August 13, 2025

Hi, i am using a 8GB Intenso class 10 microSD card. I have used this card to run SD_ReadWrite_DMA example ( example found in STM32U3, i adjusted for STM32U5 ), It worked for Datalog2 software in MKBOXPRO_A. So, i guess it is 512 sector size. but using 512 , fx_media_open(); stucks, only minimum this line the fx_media_open() works

#define FX_STM32_SD_DEFAULT_SECTOR_SIZE 2*512

 

frogrammer_0-1755081346889.png

 

Saket_OmBest answer
Technical Moderator
August 13, 2025
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"