Skip to main content
RFlod.2
Associate III
October 3, 2025
Solved

STM31L431 RTC calibration with LSI

  • October 3, 2025
  • 1 reply
  • 265 views

I need to calibrate STM32l431 RTC in software for using LSI clock.

 

When I compare STM32 RTC with GPS reference I get the following 

GPS 1759492828 1759493307 => RTC 1759500022 1759500494
Diff GPS: 479 seconds
Diff STM32: 472 seconds
=> 7 seconds = 1.48% difference and
Prefered frequency to RTC 32473

 

I thought smooth calibration could be used for this kind of calibration but it seems it can only calibrate small changes for crystal.

Any ideas how this can be done? I cannot modify PCB for external pulses, I need to correct in software.

 

Clock will be syncronised 8, 16  and 24 hours interval, so accuracy does not need to be like a crystal.

Best answer by mbarg.1

As in previous mail:

your dividers are (127 + 1) * (255 + 1) = 32768 !

if you want to use 32kHz, move async divider to 124 (count 125) and get:

dividers (124 + 1) * (255 + 1) = 32000.

Than you can trim.

1 reply

mbarg.1
Senior III
October 3, 2025

LSI is NOT 32768 but 32000 Hz

You have to change pre-scaler in RTC. I guess async prescaler should be 124 (count 125) instead of 127 (count 128).

Print RTC actual registers and let us discuss, i do not have any L4 to make a screenshot.

 

Please mark as solution if it works for you.

RFlod.2
RFlod.2Author
Associate III
October 3, 2025

Yes LSI frequency is 32000 Hz. 

 

This is RTC init:

/* Configure RTC */
	RTCHandle.Instance = RTC;
	/* Set the RTC time base to 1s */
	/* Configure RTC prescaler and RTC data registers as follow:
	- Hour Format = Format 24
	- Asynch Prediv = Value according to source clock
	- Synch Prediv = Value according to source clock
	- OutPut = Output Disable
	- OutPutPolarity = High Polarity
	- OutPutType = Open Drain */
	RTCHandle.Init.HourFormat = RTC_HOURFORMAT_24;
	RTCHandle.Init.AsynchPrediv = 127;
	RTCHandle.Init.SynchPrediv = 255;
	RTCHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
	RTCHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
	RTCHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;

	HAL_RTC_Init(&RTCHandle);

	LL_RTC_TIME_SetFormat(RTC, LL_RTC_HOURFORMAT_24HOUR);
	LL_RTC_TIME_Init(RTC, LL_RTC_FORMAT_BIN, &time);
	LL_RTC_DATE_Init(RTC, LL_RTC_FORMAT_BIN, &date);

	rtcSet = false;

 

 

I would like to calculate the prescaler based om measured GPS diff, since it will be different on different CPU and different temperatures

 

mbarg.1
mbarg.1Best answer
Senior III
October 3, 2025

As in previous mail:

your dividers are (127 + 1) * (255 + 1) = 32768 !

if you want to use 32kHz, move async divider to 124 (count 125) and get:

dividers (124 + 1) * (255 + 1) = 32000.

Than you can trim.