Skip to main content
Associate II
June 20, 2025
Solved

STM32 ADC + DMA does not update value

  • June 20, 2025
  • 5 replies
  • 853 views

Board: NUCLEO-144 STM32H723ZG

I'm using ADC_3 with 8-bit resolution, trying to measure an analog sine wave of 1 kHz as a stimulus.

I'm trying to use the ADC with DMA. However, I am unable to get any values other than zero. I have tested it in polling mode and have successfully gotten correct values. I have been looking at multiple code examples. It seems like HAL_ADC_START_DMA should be enough to start sampling; however, my buffer isn't being updated. Where have I gone wrong?

 

DMA settings

_summer_intern__0-1750425468272.png

ADC DMA settings

_summer_intern__1-1750425517606.png

ADC_settings

_summer_intern__2-1750425596843.png

 

ADC_regular_conversionMode

_summer_intern__4-1750425625042.png

 

CODE:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "fatfs.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stm32h7xx.h"
#include "stm32h7xx_hal_uart.h"
#include "string.h"
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc3;
DMA_HandleTypeDef hdma_adc3;

SD_HandleTypeDef hsd2;

UART_HandleTypeDef huart8;
UART_HandleTypeDef huart3;

/* USER CODE BEGIN PV */
uint32_t adc_val = 0;
uint8_t adc_buff[4];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_SDMMC2_SD_Init(void);
static void MX_UART8_Init(void);
static void MX_ADC3_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MPU Configuration--------------------------------------------------------*/
 MPU_Config();

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */
 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_USART3_UART_Init();
 MX_SDMMC2_SD_Init();
 MX_UART8_Init();
 MX_FATFS_Init();
 MX_ADC3_Init();
 /* USER CODE BEGIN 2 */
 HAL_ADC_Start_DMA(&hadc3,&adc_val, 2);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 snprintf(adc_buff, 4,"%d",adc_val);
 adc_buff[3] = '\n';
 HAL_UART_Transmit(&huart3, adc_buff, 4,HAL_MAX_DELAY);
 HAL_Delay(1000);

 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = 64;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 34;
 RCC_OscInitStruct.PLL.PLLP = 1;
 RCC_OscInitStruct.PLL.PLLQ = 3;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 3072;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC3_Init(void)
{

 /* USER CODE BEGIN ADC3_Init 0 */

 /* USER CODE END ADC3_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC3_Init 1 */

 /* USER CODE END ADC3_Init 1 */

 /** Common config
 */
 hadc3.Instance = ADC3;
 hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc3.Init.Resolution = ADC_RESOLUTION_8B;
 hadc3.Init.DataAlign = ADC3_DATAALIGN_RIGHT;
 hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc3.Init.LowPowerAutoWait = DISABLE;
 hadc3.Init.ContinuousConvMode = ENABLE;
 hadc3.Init.NbrOfConversion = 1;
 hadc3.Init.DiscontinuousConvMode = DISABLE;
 hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc3.Init.DMAContinuousRequests = ENABLE;
 hadc3.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
 hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
 hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc3.Init.OversamplingMode = DISABLE;
 hadc3.Init.Oversampling.Ratio = ADC3_OVERSAMPLING_RATIO_2;
 if (HAL_ADC_Init(&hadc3) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_5;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC3_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 sConfig.OffsetSign = ADC3_OFFSET_SIGN_NEGATIVE;
 if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC3_Init 2 */

 /* USER CODE END ADC3_Init 2 */

}

/**
 * @brief SDMMC2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_SDMMC2_SD_Init(void)
{

 /* USER CODE BEGIN SDMMC2_Init 0 */

 /* USER CODE END SDMMC2_Init 0 */

 /* USER CODE BEGIN SDMMC2_Init 1 */

 /* USER CODE END SDMMC2_Init 1 */
 hsd2.Instance = SDMMC2;
 hsd2.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
 hsd2.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
 hsd2.Init.BusWide = SDMMC_BUS_WIDE_4B;
 hsd2.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
 hsd2.Init.ClockDiv = 0;
 /* USER CODE BEGIN SDMMC2_Init 2 */

 /* USER CODE END SDMMC2_Init 2 */

}

/**
 * @brief UART8 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_UART8_Init(void)
{

 /* USER CODE BEGIN UART8_Init 0 */

 /* USER CODE END UART8_Init 0 */

 /* USER CODE BEGIN UART8_Init 1 */

 /* USER CODE END UART8_Init 1 */
 huart8.Instance = UART8;
 huart8.Init.BaudRate = 9600;
 huart8.Init.WordLength = UART_WORDLENGTH_8B;
 huart8.Init.StopBits = UART_STOPBITS_1;
 huart8.Init.Parity = UART_PARITY_NONE;
 huart8.Init.Mode = UART_MODE_TX_RX;
 huart8.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart8.Init.OverSampling = UART_OVERSAMPLING_16;
 huart8.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart8.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart8.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart8, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart8, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart8) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN UART8_Init 2 */

 /* USER CODE END UART8_Init 2 */

}

/**
 * @brief USART3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART3_UART_Init(void)
{

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 huart3.Instance = USART3;
 huart3.Init.BaudRate = 9600;
 huart3.Init.WordLength = UART_WORDLENGTH_8B;
 huart3.Init.StopBits = UART_STOPBITS_1;
 huart3.Init.Parity = UART_PARITY_NONE;
 huart3.Init.Mode = UART_MODE_TX_RX;
 huart3.Init.HwFlowCtl = UART_HWCONTROL_RTS_CTS;
 huart3.Init.OverSampling = UART_OVERSAMPLING_16;
 huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream0_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */
 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GNSS_NRST_GPIO_Port, GNSS_NRST_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, LED_GREEN_Pin|LED_RED_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOG, SD_EN_Pin|SD_SEL_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : GNSS_PPS_Pin */
 GPIO_InitStruct.Pin = GNSS_PPS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GNSS_PPS_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : GNSS_NRST_Pin */
 GPIO_InitStruct.Pin = GNSS_NRST_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GNSS_NRST_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : LED_GREEN_Pin LED_RED_Pin */
 GPIO_InitStruct.Pin = LED_GREEN_Pin|LED_RED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : SD_CD_Pin */
 GPIO_InitStruct.Pin = SD_CD_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(SD_CD_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : SD_EN_Pin SD_SEL_Pin */
 GPIO_InitStruct.Pin = SD_EN_Pin|SD_SEL_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */
 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

 /* MPU Configuration */

void MPU_Config(void)
{
 MPU_Region_InitTypeDef MPU_InitStruct = {0};

 /* Disables the MPU */
 HAL_MPU_Disable();

 /** Initializes and configures the Region and the memory to be protected
 */
 MPU_InitStruct.Enable = MPU_REGION_ENABLE;
 MPU_InitStruct.Number = MPU_REGION_NUMBER0;
 MPU_InitStruct.BaseAddress = 0x0;
 MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
 MPU_InitStruct.SubRegionDisable = 0x87;
 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
 MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

 HAL_MPU_ConfigRegion(&MPU_InitStruct);
 /* Enables the MPU */
 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

 

Best answer by _summer_intern_

Ended up using the linker script to set of some memory. This solved the problem. look here https://controllerstech.com/stm32-adc-multiple-channels-circular-dma/

5 replies

Karl Yamashita
Principal
June 21, 2025

You need to calibrate the ADC before starting the DMA

 

HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET /* or ADC_CALIB_OFFSET_LINEARITY*/ , ADC_SINGLE_ENDED);

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Andrew Neil
Super User
June 21, 2025

@_summer_intern_ wrote:

CODE:

 /* USER CODE BEGIN 2 */
 HAL_ADC_Start_DMA(&hadc3,&adc_val, 2);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 snprintf(adc_buff, 4,"%d",adc_val);
 adc_buff[3] = '\n';
 HAL_UART_Transmit(&huart3, adc_buff, 4,HAL_MAX_DELAY);
 HAL_Delay(1000);
 }

You start the ADC+DMA, and then immediately print the results.

You need to wait for the ADC acquisition and DMA transfer to complete before the results will be available! 

Also, adc_val will need to be volatile.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ozone
Principal
June 23, 2025

> You start the ADC+DMA, and then immediately print the results.

Correct. Which suggests the OP does not yet really grasp the idea of DMA, and how it works.

And this compelled me to take a look at the source code - despite the fact that Cube code hurts my eyes ...
But there is a DMA interrupt configured, but no respective callback (assuming no modifications of the default interrupt handler).
I assume this is the TC interrupt, which would be the right time to process the ADC input.

 

On a related note ...
If I do such a thing (continuous printing out ADC results via UART), I check before that the output bandwith exceeds the input bandwitdh. I am not sure such a check happened here.

Technical Moderator
June 23, 2025
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Karl Yamashita
Principal
June 24, 2025

@_summer_intern_ 

I missed it earlier but I see that you have Continuous Conversion Mode enabled. In previous projects, I observed that this will cause interrupts continuously to the point the ADC can't do a conversion correctly.

So I did a test again and I was able to replicate your issue with ADC1 with Continuous Conversion Mode enabled. It was reporting 0, as you've indicated.

 

To fix it do this. I created a 100ms interrupt timer to trigger the ADC conversion.

1. In ADC, disable Continuous Conversion Mode

2. Enable a timer like Timer15.

  1. Enable Internal Clock.
  2. Enable auto-reload preload
  3. Set Trigger Event Selection for Update Event.
  4. Set period (and Prescaler) to a value to get interrupts like between 100ms to 1us. Anything faster might be too much overhead, but then it also depends on your clock speed.

3. Now in ADC,  set External Trigger Conversion Source to Timer 15, Trigger Out Event

 

 

int main(void)
{
// other HAL code

 /* USER CODE BEGIN 2 */
 uint16_t adc_val;
 char str[16];
 HAL_ADCEx_Calibration_Start(&hadc1);
 HAL_ADC_Start_DMA(&hadc1,(uint32_t*)&adc_val, 1); // only 1 conversion/rank
 HAL_TIM_Base_Start_IT(&htim15); // set for 100ms interrupts
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 HAL_Delay(1000); // allow for first conversion to complete
	 sprintf(str, "%d\n", adc_val);
	 HAL_UART_Transmit(&huart2, (uint8_t*)str, strlen(str), 100);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Ozone
Principal
June 24, 2025

> I missed it earlier but I see that you have Continuous Conversion Mode enabled. In previous projects, I observed that this will cause interrupts continuously to the point the ADC can't do a conversion correctly.

I missed that, too.
Probably because the idea doesn't make too much sense in the first place - continuous single-channel conversion with DMA.
The "old" SPL examples mostly used continuous conversion, pushed the value in a buffer variable, and the main loop read at irregular intervals.

> To fix it do this. I created a 100ms interrupt timer to trigger the ADC conversion.
> 1. In ADC, disable Continuous Conversion Mode
> 2. Enable a timer like Timer15.
> ...

An approved method that works quite well.
I don't know the H7 variant, but most F0...F7 ADCs have options to trigger an ADC conversion from a timer directly, in the ADC peripheral config register. The exact timer device depends on the variant.

DMA, at least for a real application, makes sense for multiple channels.
In this case, the DMA TC interrupt would be the place to pick up the results.

_summer_intern_AuthorBest answer
Associate II
July 2, 2025

Ended up using the linker script to set of some memory. This solved the problem. look here https://controllerstech.com/stm32-adc-multiple-channels-circular-dma/