Skip to main content
Associate
May 21, 2025
Question

STM32 ISP-IQTune Port Detection Issue with IMX335 on STM32N657X0H3Q

  • May 21, 2025
  • 3 replies
  • 712 views

大家好!

问题是这样的: 

我正在尝试使用 STM32 ISP-IQTune 应用程序通过 STM32N657X0H3Q 板读取 PC 上的 IMX335 相机数据。但是,IQTune 无法检测到任何可用的 COM 端口。这是我的设置:

  • 硬件:
    • 板:STM32N657X0H3Q
    • 相机:IMX335(MB1854B模块,根据文档提供原生支持)。
    • 固件:已从 STM32N6 固件包中刷新 DCMIPP_ContinuousMode 示例。
  • 连接:
    • 已将板上的两个 USB 端口连接到 PC(USB-C 电缆)。
    • 开发板显示红色 LED 闪烁,表示程序正在运行。

问题:
尽管板子看起来正常工作,但 ISP-IQTune 显示“未检测到端口”。我已验证:

  1. USB 电缆支持数据传输(与其他设备一起测试)。
  2. 已安装 STM32CubeIDE 驱动程序。
  3. IMX335 在 ISP-IQTune 文档中被列为兼容的传感器。

问题:

  1. 是否有其他步骤可以在 ISP-IQTune 中启用 COM 端口可见性?
  2. DCMIPP_ContinuousMode示例是否需要修改 ISP-IQTune 兼容性?
  3. 应该只连接 CN18 (USB1),还是两个 USB 端口都需要?

感谢您的时间和帮助!

3 replies

陶铸_itAuthor
Associate
May 21, 2025

Hello everyone!

The question is this: 

I’m trying to use the ​​STM32 ISP-IQTune application​​ to read the IMX335 camera data on my PC via the STM32N657X0H3Q board. However, IQTune fails to detect any available COM port. Here’s my setup:

  • ​Hardware:​
    • Board: STM32N657X0H3Q
    • Camera: IMX335 (MB1854B module, natively supported per documentation).
    • Firmware: Flashed the ​​DCMIPP_ContinuousMode​​ example from the STM32N6 firmware package.
  • ​Connections:​
    • Connected ​​both USB ports​​ on the board to the PC (USB-C cables).
    • The board shows a ​​red LED blinking​​, indicating the program is running.

​Issue:​
Despite the board seemingly functioning, ISP-IQTune shows ​​"No port detected"​​. I’ve verified:

  1. USB cables support data transfer (tested with other devices).
  2. STM32CubeIDE drivers are installed.
  3. IMX335 is listed as a compatible sensor in the ISP-IQTune documentation.

​Questions:​

  1. Are there additional steps to enable COM port visibility in ISP-IQTune?
  2. Could the DCMIPP_ContinuousMode example require modifications for ISP-IQTune compatibility?
  3. Should only ​​CN18 (USB1)​​ be connected, or are both USB ports necessary?

Thank you for your time and assistance!

Technical Moderator
May 21, 2025

Hello @陶铸_it 

Is the COM port visible on the device manager?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
陶铸_itAuthor
Associate
May 22, 2025

It is not visible in Device Manager.

We sincerely apologize for the inconvenience. Upon rechecking, we discovered that some pins on the IMX335 modules we purchased differ from the official specifications. Attached are the relevant screenshots—the left image shows the official datasheet, while the right displays the pin definitions of the purchased IMX335 modules, with the discrepancies clearly marked. We suspect this might be the reason why the module is not being detected. If so, we deeply regret any trouble caused by our oversight in the preliminary preparations.

Additionally, we would like to inquire whether it is mandatory to use ST's official camera module, given its high cost. We are exploring alternative solutions, such as:

  1. If the issue is merely a pin order mismatch, could we rewire the 22 pins from N6 using pin headers and sockets? If connected this way, would it still be possible to read data via USB and IQTune?
  2. If a custom configuration for a different camera is required, do you have any recommendations? We noticed that the X-CUBE-ISP beginner tutorials provide limited guidance on such adaptations, and we are concerned about potential hardware/software compatibility issues that might hinder image transmission.

Thank you for taking the time to address our concerns. We greatly appreciate your assistance!

Associate
September 9, 2025

Hi Team , 
               I am also using ISP-IQ Tune tool to tune IMX219 Sensor , I'm too getting same issue , not able to detect the port , Can you tell how did you solve the issue?

I am able to stream camera using Camera ISP Preview.

Visitor II
November 5, 2025

大家好,

1,我也在使用ISP-IQ Tune工具来调优IMX335传感器,遇到了同样的问题,无法检测到端口。请问你们是如何解决这个问题的?

2,windows 上是可以识别到COM口的

chris10_0-1762309204030.png

3,COM29 没有被占用,ISP-IQ Tune 仍是无法识别

 

chris10_1-1762309246511.png