STM32 USB Audio Class
Hello,
I need to build a USB headset(mic+speaker) using STM32H742VIT6 for a project. I want the stm32h7 to be recognized as a audio device when connected to a PC/android device. Is this possible?
This is my first time using a STM Board with cubeMX and cubeIDE, so I want to build the microphone part first. I am having trouble programming the board, specially what middleware to use, how the structure of the project works in the ide, what would be the setup e.g. clock config, dma, adc, timer configuration. It would be nice if I could get some resources/guide on how to start, because I am lost inside the mx and ide!
Hardware:
WeAct Studion STM32H742VIT6
MAX4466 mic