STM32 USB HID + VCP not working but DFU is
I am using the STM32L433 MCU and both the HID and VCP interfaces are not working even though the DFU is.
I am simply using the STM32CubeMX software to generate a standard default USB Setup but I keep getting the same Windows USB Error "USB Device Not Recognised" which is the "Device Descriptor request failed".
My hardware is a custom design and believe that I have the correct differential impedance or the DFU would not have worked.
VBUS is at 3.3V (<4V)
D+/D- traces > 2 inches but differential impedance has been matched to 90 Ohms using Altium.
I have a 12MHZ Crystal, the MCU can run Crystal-less.
USB is 48MHz but runs from RC, also used PLLSA1 from HSE.
STM32CubeIDE v2.1.1
MX_USB_DEVICE_Init() called.
If the DFU is working then why not the other USB Interfaces?