STM32C0 USBX CDC send data un-stoppable
Hello, I am using STM32C071 in my project, the main work is to receive data from PC, then do some controls, then send data to PC.
However, during the send data to PC step, sometimes the data will be sent continuously, it doesn't meet my requirements, sometimes it working well, this is very unusual. please provide some advise.
After I send the data and proceduce the 'handleRecvData()' func, the data I received from PC is not un-stoppable.
I have checked several days and I can't find what caused this ab-normal.

I follow the steps from
the write and read threads code shows as below:
/* Private function prototypes -----------------------------------------------*/
/* USER CODE BEGIN PFP */
uint8_t resultCode = 0;
extern TX_MUTEX mutexCode;
/* USER CODE END PFP */
VOID usbx_cdc_acm_write_thread_entry(ULONG thread_input)
{
/* Private Variables */
ULONG tx_actual_length;
uint8_t initGoodMsg[] = "Init Good!";
uint8_t opGoodMsg[] = "Operate Good!";
uint8_t opErrorMsg[] = "Operate Error!";
uint8_t headerErrorMsg[] = "Header Error!";
uint8_t flameErrorMsg[] = "Flame Error!";
uint8_t msgToSend[15];
while(1)
{
if(tx_mutex_get(&mutexCode, TX_WAIT_FOREVER) == TX_SUCCESS){
while(resultCode != 0){
switch(resultCode){
case initGood:
memcpy(msgToSend, initGoodMsg, sizeof(initGoodMsg));
break;
case opGood:
memcpy(msgToSend, opGoodMsg, sizeof(opGoodMsg));
break;
case opError:
memcpy(msgToSend, opErrorMsg, sizeof(opErrorMsg));
break;
case headerError:
memcpy(msgToSend, headerErrorMsg, sizeof(headerErrorMsg));
break;
case flameError:
memcpy(msgToSend, flameErrorMsg, sizeof(flameErrorMsg));
break;
default:
break;
}
resultCode = 0;
ux_device_class_cdc_acm_write(cdc_acm, (UCHAR *)(msgToSend), sizeof(msgToSend), &tx_actual_length);
}
}
tx_mutex_put(&mutexCode);
tx_thread_sleep(150);
}
}
VOID usbx_cdc_acm_read_thread_entry(ULONG thread_input)
{
/* Private Variables */
ULONG rx_actual_length;
uint8_t UserRxBuffer[10];
/* Infinite Loop */
while(1)
{
if(cdc_acm != UX_NULL)
{
ux_device_class_cdc_acm_read(cdc_acm, (UCHAR *)UserRxBuffer, 10, &rx_actual_length);
if(rx_actual_length != 0){
if(tx_mutex_get(&mutexCode, TX_WAIT_FOREVER) == TX_SUCCESS){
//handle receive data
handleRecvData((uint8_t *)UserRxBuffer, rx_actual_length);
tx_mutex_put(&mutexCode);
}
}else{
tx_thread_sleep(100);
}
}
tx_thread_sleep(100);
}
}VOID handleRecvData(uint8_t *RecvRxBuffer, ULONG bufferLength)
{
if((RecvRxBuffer[0] == 0xAA) && (RecvRxBuffer[1] == 0xCC) && (RecvRxBuffer[bufferLength-2] == 0xAA) && (RecvRxBuffer[bufferLength-1] == 0x55))
{
// 帧头帧尾 OK
if(RecvRxBuffer[2] == (bufferLength - 4)){
// 帧长确认OK
switch(RecvRxBuffer[3]) // 功能位
{
case 0x00:
resultCode = 1;
HAL_NVIC_SystemReset();
break;
case 0x01:
if(boardInit() == HAL_OK){
resultCode = initGood;
}
else{
resultCode = opError;
}
break;
case 0x02:
if(setFingerCh(RecvRxBuffer[4], RecvRxBuffer[5], RecvRxBuffer[6]) == HAL_OK){
resultCode = opGood;
}
else{
resultCode = opError;
}
break;
default:
resultCode = flameError;
break;
}
}else{
// 帧长错误
resultCode = flameError;
}
}else{
// 帧头帧尾 error
resultCode = headerError;
}
}