Skip to main content
Associate II
May 20, 2025
Solved

STM32CubeMX - V6.12.0 CAN-FD Transciever Delay Compensation & Auto Retransmission

  • May 20, 2025
  • 2 replies
  • 661 views

Hi,

I'm currently using STM32CubeMX V6.12.0 to initialise the peripherals on an STM32H753 processor, and I had a couple of questions:

1. How do I enable & then configure the CAN Transciever Delay Compensation within CubeMX?

2. Is there a mechanism for limiting the number of auto-retransmissions in the event of a CAN Error? I currently have that option unchecked but when doing bench-top testing it's clogging up the processor and causing it to run slowly.

 

Many Thanks,

 

Crispin

Best answer by Semer CHERNI

Hello @CZuercher_Ilm 

First let me thank you for posting.

About the CAN Transciever Delay Compensation, it is not possible to configure it from within STM32CubeMX.

For more details, I will redirect your question to the STM32MCUs forum as it is a better place to get help with the CAN configuration.

KR,
Semer.

2 replies

Semer CHERNI
Semer CHERNIBest answer
ST Employee
May 23, 2025

Hello @CZuercher_Ilm 

First let me thank you for posting.

About the CAN Transciever Delay Compensation, it is not possible to configure it from within STM32CubeMX.

For more details, I will redirect your question to the STM32MCUs forum as it is a better place to get help with the CAN configuration.

KR,
Semer.

Technical Moderator
May 23, 2025

@CZuercher_Ilm wrote:

2. Is there a mechanism for limiting the number of auto-retransmissions in the event of a CAN Error? I currently have that option unchecked but when doing bench-top testing it's clogging up the processor and causing it to run slowly.


You can disable completely the retransmission with Init.AutoRetransmission = DISABLE.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Associate II
May 28, 2025

Hi Saket,

 

Yes; I have disabled this particular bit of functionality, however in the fullness of time I need to be able to limit the number of retransmission attempts to say, 6, before that message is abandoned.

Is there a way of doing this elegantly and efficiently, without having to call interrupts etc.?

 

Many Thanks,

 

Crispin