Skip to main content
Associate II
September 28, 2025
Question

STM32F4 + SDIO + FATFS

  • September 28, 2025
  • 1 reply
  • 306 views

Hello,

I am trying to get f_mount() to work with the SDIO peripheral.

 

Currently, the f_mount() reaches the first disk_read() function, where it hangs in the osMessageQueueGet() call. 

 

Stuff I already tried:

- increase min & max heap to 0x400, 0x800

- increase default static rtos task stack size to 8000

- call f_mount in the default task

- have delay before f_mount

- pullup on all IO pins except the CLK

- the hsd.Instance has recognized card type and class

- the NVIC prio is 5 for SDIO and DMA stream

- tried SDIO_RX/SDIO_TX combo and just SDIO

- tried setting GPIO pins to lower speeds

- tried SD bit 1 mode and then switching to 4bit mode

- tried SD bit 1 mode and keeping 1 bit mode

- SDIO_IRQ interrupt hits, but does not put anything in the SDQueueID queue.

 

i would prefer to use the cubemx generated drivers and not write one myself. is this configuration (RTOS+SDIO+FATFS) not possible/bugged?

 

thanks.

1 reply

Technical Moderator
September 29, 2025

Hello @ayhamxyz 

Please refer to the example below as starting point.

STM32CubeF4/Projects/STM324x9I_EVAL/Applications/FatFs/FatFs_uSD_RTOS at master · STMicroelectronics/STM32CubeF4 · GitHub


@ayhamxyz wrote:

- the NVIC prio is 5 for SDIO and DMA stream

 


The interrupt priority is too high (must be lower than the RTOS kernel interrupt priority which is 5).

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
ayhamxyzAuthor
Associate II
September 30, 2025

I tried that with no avail,

 

I am using the automatically generated SDIO dma template driver from stm32cubemx/ide, which follows closely the project @Saket_Om linked, except that I am using CMSISv2, so it is using the newer osQueue* functions.

 

I tried to use f_mount() with a new project, no rtos, no dma, and that did not work. I used 2 different SDcards, both are SanDisk, one is a newer 128gb and another is 32gb (older HD version). The SDIOCLK divisor is 4, so that should work.

 

I am starting to suspect that it is a PCB issue.

 

Thanks for your reply anyhow.