Skip to main content
Eich
Associate III
July 25, 2013
Question

STM32F405RG VCP error ''This device cannot start(code 10)''

  • July 25, 2013
  • 12 replies
  • 10459 views
Posted on July 25, 2013 at 11:26

Hi !

When running the VCP USB Stack (STM32_USB-Host-Device_Lib_V2.1.0) on my STM32F4 i got an error code on my Win7 x64 sytem. ''This device cannot start(code 10)'' I'm using the USB HS Port on PORTB in FS mode. Finally i found a solution for it. The source code of the file usbd_conf.h must be changed in the following way: Old:

/* CDC Endpoints parameters: you can fine tune these values depending on the needed baudrates and performance. */
#ifdef USE_USB_OTG_HS
#define CDC_DATA_MAX_PACKET_SIZE 512 /* Endpoint IN & OUT Packet size */
#define CDC_CMD_PACKET_SZE 8 /* Control Endpoint Packet size */

New

/* CDC Endpoints parameters: you can fine tune these values depending on the needed baudrates and performance. */
#ifdef USE_USB_OTG_HS
#define CDC_DATA_MAX_PACKET_SIZE 64 /* Endpoint IN & OUT Packet size */
#define CDC_CMD_PACKET_SZE 8 /* Control Endpoint Packet size */

This change is only necessary when using the HS USB in FS mode. Regards, Ed #stm32-stm32f4-vcp-otg_hs-usb

12 replies

Nickname12657_O
Associate III
July 25, 2013
Posted on July 25, 2013 at 21:53

Hi Ed,

Much appreciated!  All thanks from STMicro.

Cheers,

STOne-32

2dimka
Visitor II
December 28, 2014
Posted on December 28, 2014 at 20:48

Hi! I have a same problem with VCP. But i can't install driver for built-in virtual com port on ST-LinkV2 (Nucleo board).

I use latest version of ST firmware and drivers, and my OS is Windows XP x64 sp3.

Whether you can help me? thanks.

em3ly
Associate
November 9, 2015
Posted on November 09, 2015 at 23:25

Hi, i had the same problem. Thanks for help me to  fix my problem. I'm using STM32CubeMx and STM32F4 Discovery. In the stm32CubeMx proyect I configure correctly the usb clock (48MHz) and  i'm using usb_otg_fs as device only. The solution  for ''This device cannot start(code 10)'' is almost the same that in your case.

 In the source code of ''usbd_cdc.h''  must be changed 

#define CDC_DATA_HS_MAX_PACKET_SIZE                512  /* Endpoint IN & OUT Packet size */

 to

#define CDC_DATA_HS_MAX_PACKET_SIZE                 64  /* Endpoint IN & OUT Packet size */

I hope  it help somebody

Cevdet
Associate III
January 29, 2019

Yes, it helped, thank you for sharing:)

But I am wondering why ? I don't even use HS... what did changed by this definition?

MHoga
Visitor II
March 7, 2019
typedef struct
{
 uint32_t data[CDC_DATA_HS_MAX_PACKET_SIZE / 4U]; /* Force 32bits alignment */
 uint8_t CmdOpCode;
 uint8_t CmdLength;
 uint8_t *RxBuffer;
 uint8_t *TxBuffer;
 uint32_t RxLength;
 uint32_t TxLength;
 
 __IO uint32_t TxState;
 __IO uint32_t RxState;
}
USBD_CDC_HandleTypeDef;

It seems regardless whether you are using FS or HS, CDC_DATA_HS_MAX_PACKET_SIZE is used to define this type, I am just an electronics intern so don't have much experience at the moment but it seems to be issue, as when I replace it with what is below, it seems to also work, if anyone is able to explain to me why, it would be helpful

typedef struct
{
 uint32_t data[64U]; /* REPLACEMENT */
 uint8_t CmdOpCode;
 uint8_t CmdLength;
 uint8_t *RxBuffer;
 uint8_t *TxBuffer;
 uint32_t RxLength;
 uint32_t TxLength;
 
 __IO uint32_t TxState;
 __IO uint32_t RxState;
}
USBD_CDC_HandleTypeDef;

aaron239955_stm1_st
Senior
November 13, 2015
Posted on November 13, 2015 at 12:05

you don't indicate what version of cube or libraries you are using.  I believe if you update to a recent version (1.8.0 or later) of the F4 libraries this problem has been fixed for over a year.  You shouldn't have to do any changes to the usbd_cdc.h file

enjoy

tsuneo
Associate II
December 29, 2015
Posted on December 29, 2014 at 06:31

> But i can't install driver for built-in virtual com port on ST-LinkV2 (Nucleo board).

Install the latest PC driver for ST-LINK/V2-1, first.

STSW-LINK008   ST-LINK/V2-1 USB driver on Windows Vista, 7 and 8

http://www.st.com/web/en/catalog/tools/FM147/SC1887/PF260218

STSW-LINK009   ST-LINK/V2-1 USB driver on Windows XP (including WinUSB coinstallers)

http://www.st.com/web/en/catalog/tools/FM147/SC1887/PF260219

OR

you may need to update ST-LINK/V2-1 firmware on your Nucleo board.

STSW-LINK007   ST-LINK/V2-1 firmware upgrade

http://www.st.com/web/en/catalog/tools/FM147/SC1887/PF260217

Tsuneo

sycinfinity
Associate
May 11, 2016
Posted on May 11, 2016 at 04:37

Thank you for your commend. 

I spend all day to solve this problem. and I change CDC_DATA_HS_MAX_PACKET_SIZE 512 => 64,

my VCP driver work well.

Sami.Oweis
Associate
March 21, 2019

Thank you Eichel.

I was inspired by ur solution and was able to resolve my issue with a different library version.

Here is for anyone is still have the same issue.

https://community.st.com/s/question/0D50X0000AX88PpSQJ/stm32f4x-stmicroelectronics-virtual-com-port-is-properly-installed-but-cant-start-error-this-device-cannot-start-code-10-win7-64fixed

mmed
Associate III
March 26, 2019

Hi all,

using windows10,

I want to handle STM32F407 Disco via VCP. In the first case, i tried to configure UART but when i connect my USB TTL converter to my PC: it informs me that VCP error ''This device cannot start(code 10)''.

I thought that the probem is related to my USB converter

Then i tried to configure CDC USB:

USB_OTG_FS on mode Device only

activate USB_Device middelware in CDC mode

0690X0000088qxcQAA.png

check the CubeMX file attached for more details

but the problem still exist!===> VCP error ''This device cannot start(code 10)''.

0690X0000088qxSQAQ.png

and here is the define in "usbd_desc.c" file

#define USBD_VID   1155

#define USBD_LANGID_STRING   1033

#define USBD_MANUFACTURER_STRING   "STMicroelectronics"

#define USBD_PID_FS   22336

#define USBD_PRODUCT_STRING_FS   "STM32 Virtual ComPort"

#define USBD_SERIALNUMBER_STRING_FS   "00000000001A"

#define USBD_CONFIGURATION_STRING_FS   "CDC Config"

#define USBD_INTERFACE_STRING_FS   "CDC Interface"

=====> Please how can i handle to fix this issue! if there is a wrong value generated by CubeMX! or a change that should i do in my environement (PID, VID....)

this is a real problem for me that block my project0

Please any solution or workaround for this

many thanks

H W
Associate II
July 26, 2019

Having the same problem under Win 10 with a STM32L476 and Firmware 1.14.0 !

(USB-Sniffer: device answers correctly after DESCRIPTOR Request DEVICE from host. After DESCRIPTOR Request CONFIGURATION the device returns the correct information, but the device status is USBD_STATUS_STALL_PID (0xc0000004 -> 'error 10 device cannot start') and no further communication)

Any help ?

finnstap
Visitor II
September 3, 2019

Hi, I have the same problem with the STM32L496 and firmware 1.14.0, also Win 10. Actually the device managed to enumerate successfully once and I was able to view incoming data with putty. I have no idea, why that happened.. Most of the time, the configuration descriptor is invalid (USBD_STATUS_STALL_PID (0xc0000004)). Were you able to fix this?

finnstap
Visitor II
February 4, 2020

Hey, just a quick follow up, I tested my solution thoroughly and after making sure it has no negative effects on the usb transmission I finally submitted a bug report to github: https://github.com/STMicroelectronics/STM32CubeH7/issues/22

tl;dr the bug is known and will be fixed in the new upcoming USB device lib.

RMa.1
Visitor II
June 14, 2020

Just run into a similar issue with STM32F405xx.

Thanks a lot for the folks here for the hint.

For me the issue is the same as Eich mentioned: Changing CDC_DATA_HS_MAX_PACKET_SIZE from 512U to 64U solve the problem.

I took a look at the issue and found that:

  1. In the usbd_cdc.c, USBD_CDC_Init() is using this value to allocate memory: USBD_malloc(sizeof(USBD_CDC_HandleTypeDef));
  2. the USBD_malloc is by default using malloc of the compiler... which means it takes heap.
  3. I checked my default linker directive and found the heap size is 0x200 (512 bytes)
  4. This is certainly going to cause trouble....and lucky me only run into a USB error not other issues....

If you do not like the solution to change the CDC_DATA_HS_MAX_PACKET_SIZE from 512 to 64 (like me...), you can enlarge the heap size by modifying the link directive file.

In my case, I am using IAR, I changed heap to 8KBytes:

define symbol __ICFEDIT_size_heap__  = 0x2000;