STM32F469AIHX: fails when using Bootloader + Application split at over 128Mhz
I am developing firmware with a Boot region and Application region split for OTA firmware update on STM32F469AIHX.
[Environment]
- MCU: STM32F469AIHX (Max core clock: 180MHz)
- IDE: STM32CubeIDE
- HAL Library: STM32CubeF4
- Flash layout: Bootloader (Sector 0~N) / Application (Sector N+1~)
[Problem]
When the flash is split into Boot and App regions, the system does not operate correctly at 180MHz.
However, setting the core clock to 128MHz works fine.
Also, the Application running alone from address 0x08000000 works fine at 180MHz.
[What I have already tried]
- Reset CubeMX configuration to default, only changed flash memory layout
- Verified VTOR is correctly set to APPLICATION_ADDRESS
- Verified SysTick_Handler calls HAL_IncTick()
- Confirmed uwTick does not increment when running at 180MHz after jump
- Removed HAL_RCC_DeInit() / HAL_DeInit() before jump in bootloader
- Tried setting SCB->VTOR before HAL_Init() in application main()
[Bootloader jump code]
__disable_irq();
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
SCB->VTOR = APPLICATION_ADDRESS;
JumpAddress = *(__IO uint32_t*)(APPLICATION_ADDRESS + 4);
JumpToApplication = (pFunction)JumpAddress;
__set_MSP(*(__IO uint32_t*)APPLICATION_ADDRESS);
JumpToApplication();[Question]
1. Why does 180MHz fail only when Boot+App split is used?
2. Is there any specific RCC or Flash latency configuration required when jumping from bootloader to application?
3. Could Flash wait states (FLASH_ACR latency) be the root cause?
Any advice would be greatly appreciated.
Thank you.