Skip to main content
Associate III
July 12, 2025
Solved

STM32F767 QSPI Flash Not Writing First Byte (S25FL256S)

  • July 12, 2025
  • 1 reply
  • 377 views

Hi everyone,

I'm using an STM32F767 with an S25FL256S NOR flash over QSPI in indirect mode (HAL driver).

I'm trying to write the string "HELLO" at address 0x000000, but after programming and reading, I always get: FF 45 4C 4C 4F → "ELLO".

The first byte is always 0xFF. All other bytes are written and read correctly.

 

What I’ve already done:

  • Verified Flash ID: 01 20 18 (correct)

  • Erased the sector before writing

  • Using 0x02 Page Program in 1-1-1 mode

  • Set SIOOMode = QSPI_SIOO_INST_ONLY_FIRST_CMD

  • Set FIFO threshold = 1

  • Using indirect mode (HAL_QSPI_Command() + HAL_QSPI_Transmit())

  •  

  • Test Code:
    char tx[] = "HELLO";
    QSPI_PageProgram(0x000000, (uint8_t*)tx, strlen(tx) + 1);
    QSPI_ReadData(0x000000, rx, strlen(tx) + 1);

    Why is the first byte not being written?

Best answer by MHoll.2

Accoding to the S25FL256S Datasheet the 0x13 read command needs a 32 Bit Address, but You are sending only 24 Bit.

MHoll2_1-1752328889322.png

 

/*------------------------------------------------------------
 QSPI_ReadData
 Reads data starting at the given 24-bit address using the Read Data command (0x03).
 Datasheet reference: Section 11.4.1 (Normal Read).
------------------------------------------------------------*/
HAL_StatusTypeDef QSPI_ReadData(uint32_t address, uint8_t *pData, uint32_t Size)
{
 sCommand.Instruction = CMD_READ_DATA;
 sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
 sCommand.Address = address;
 sCommand.AddressMode = QSPI_ADDRESS_1_LINE;
 sCommand.AddressSize = QSPI_ADDRESS_24_BITS;
 sCommand.DataMode = QSPI_DATA_1_LINE;
 sCommand.DummyCycles = 0; // Normal read does not require dummy cycles
 sCommand.NbData = Size;

 if(HAL_QSPI_Command(&hqspi, &sCommand, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 return HAL_ERROR;

 return HAL_QSPI_Receive(&hqspi, pData, HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
}

 

1 reply

MHoll.2
MHoll.2Best answer
Senior III
July 12, 2025

Accoding to the S25FL256S Datasheet the 0x13 read command needs a 32 Bit Address, but You are sending only 24 Bit.

MHoll2_1-1752328889322.png

 

/*------------------------------------------------------------
 QSPI_ReadData
 Reads data starting at the given 24-bit address using the Read Data command (0x03).
 Datasheet reference: Section 11.4.1 (Normal Read).
------------------------------------------------------------*/
HAL_StatusTypeDef QSPI_ReadData(uint32_t address, uint8_t *pData, uint32_t Size)
{
 sCommand.Instruction = CMD_READ_DATA;
 sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
 sCommand.Address = address;
 sCommand.AddressMode = QSPI_ADDRESS_1_LINE;
 sCommand.AddressSize = QSPI_ADDRESS_24_BITS;
 sCommand.DataMode = QSPI_DATA_1_LINE;
 sCommand.DummyCycles = 0; // Normal read does not require dummy cycles
 sCommand.NbData = Size;

 if(HAL_QSPI_Command(&hqspi, &sCommand, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 return HAL_ERROR;

 return HAL_QSPI_Receive(&hqspi, pData, HAL_QSPI_TIMEOUT_DEFAULT_VALUE);
}

 

MADHU2Author
Associate III
July 16, 2025

Hi @MHoll.2,

 

Yes, I tried using this command as well and observed the same issue. After checking, I noticed that the first byte is sent, but when I try to read the memory for the first time, it does not read the first byte. However, after the second read, I can read the full data bytes. So, I added a small delay, and it is now working properly.

Thank you for the help and suggestions.

 

Regards,

Madhu