Skip to main content
ADosa.1
Associate II
December 18, 2025
Solved

STM32H5 running NetXDuo with KSZ9567R

  • December 18, 2025
  • 1 reply
  • 487 views

Hello. I have two setups: one STM32H5 Nucleo eval board and a custom STM32H5 board. The Nucleo runs with the LAN8742 PHY while the eval board runs with the KSZ9567R switch. Both are configured to use RMII. 

I'm using the NetXDuo stack for both. The Nucleo board works just fine, but the custom does not. The custom board SW is based on the Nucleo SW, except removing the LAN8742 interface. 

I've checked out the HW on the custom board and it looks fine. I'm trying to do a simple ping from the PC. The first message is an ARP message. I see it on Wireshark  and it arrives just fine on the STM32. I see the MAC address and the source and destination IP which look correct in _nx_arp_packet_receive

message_type : 1
sender_physical_msw : 11352
sender_physical_lsw : 3116224427
sender_ip_address : 3232235781
target_ip_address : 3232235787

Then the SW creates the ARP reply and calls _nx_driver_packet_send. I can see the RMII Tx lines toggle after the ARP packet is sent, but for some reason the KSZ switch does not send/forward the packet back to the PC. I've looked in the memory map for both the eval board and the custom board and the ARP replies have the same message. 

Any thoughts on what it could be? Why is the LAN8742 forwarding the ARP reply while the KSZ switch does not? 

Thanks for you time.

Alin

 

Best answer by Pavel A.

Usually the factory default of these switches is "simple" - any port forwards to all others. Maybe you need to inspect per-port packet counters (a.k.a. MIB registers) to find whether the switch received the packet from STM32 and where it went to. Hope you have I2C or SPI interface to the switch.

 

1 reply

Pavel A.
Pavel A.Best answer
Super User
December 19, 2025

Usually the factory default of these switches is "simple" - any port forwards to all others. Maybe you need to inspect per-port packet counters (a.k.a. MIB registers) to find whether the switch received the packet from STM32 and where it went to. Hope you have I2C or SPI interface to the switch.

 

ADosa.1
ADosa.1Author
Associate II
December 29, 2025

Thanks Pavel. Yes, we have SPI connected so will do that next.