Skip to main content
Associate
July 15, 2025
Question

STM32H523 USBX Standalone HID Device Crashes on ux_slave_dcd_function

  • July 15, 2025
  • 2 replies
  • 394 views

I am building a device using a STM32H523RET6 microcontroller on a custom board (self-powered, with VBUS detection). My eventual goal is to operate a USB-CDC interface between the board and a computer for telemetry, but since the only standalone USB example I could find in the STM32CubeH5 examples was HID, I am trying to get a HID interface working first. I do not want to use the RTOS for my device. I have attempted to adapt the code from this example, https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/NUCLEO-H563ZI/Applications/USBX/Ux_Device_HID_Standalone to the H523 device, but the program crashes in the function _ux_device_stack_tasks_run when the function ux_slave_dcd_function is called. As you can see from the stack trace, this is called from the USBX_Device_Process() function which is periodically called. I have been unable to find any detailed information or examples pertaining to USB on the H523 device, so any information or pointers would be amazing.

nifley_0-1752558462510.png

nifley_1-1752558707376.png

I haven't changed the USBX configuration from the default aside from selecting these options.

Thanks, FB.

 

2 replies

MOBEJ
ST Employee
July 15, 2025

Hello @nifley ,

Please take a look at this article: "How to implement a USB device composite in STM32H5 microcontrollers". It provides a detailed guide that can help you configure your project using STM32CubeMX .

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
nifleyAuthor
Associate
July 15, 2025

Thanks for pointing me to that example - I don't know how I didn't find that earlier! I have adapted that example to my board; it seems that the USB device initializes, but unfortunately, my computer says that it does not recognize the device. 

nifley_0-1752599624071.png

nifley_3-1752600163891.png

 

Looking at other solutions to this problem, I have added

HAL_PWREx_EnableUSBVoltageDetector();
if (HAL_GPIO_ReadPin(VBUS_SENS_GPIO_Port, VBUS_SENS_Pin)) {
 HAL_PWREx_EnableVddUSB();
 usb_connected = true;
}

 To my initialization code, but it seems to have no effect. I'm pretty sure I have the USB lines wired properly, but I could be wrong. 

nifley_1-1752599775496.png

nifley_2-1752600012547.png

 

 

Technical Moderator
August 6, 2025

Hi @nifley 

Do you reproduce the issue using reference board for example NUCLEO-H533RE?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL