Skip to main content
Associate III
October 2, 2025
Question

STM32H747I-DISCO SAI onboard Microphone DMA error

  • October 2, 2025
  • 2 replies
  • 324 views

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code

HI 

I am having an issue with starting measurements using the on-board microphone. Everything has been configured based on the BSP code, but set up from scratch using CubeMX. The problem is that when I start the DMA Receive

 

if (HAL_SAI_Receive_DMA(&hsai_BlockA4, (uint8_t*)PDM_Buffer, PDM_BUF_SIZE) != HAL_OK)

{

printf("SAI RX start error!\r\n");

}

else

{

printf("SAI RX started OK");

}

//callbacks:

void HAL_SAI_RxHalfCpltCallback(SAI_HandleTypeDef *hsai)

{

printf("HAL_SAI_RxHalfCpltCallback\n");

}



void HAL_SAI_RxCpltCallback(SAI_HandleTypeDef *hsai)

{

printf("HAL_SAI_RxCpltCallback\n");

}



void HAL_SAI_ErrorCallback(SAI_HandleTypeDef *hsai)

{

printf("SAI error: 0x%08lx\n", hsai->ErrorCode);

}

 

I immediately get an interrupt reporting a DMA error (128 eror code in decimal).

I have already tried changing the clock frequencies, tried running it on a different core, and also tested with different data sizes, but none of this helped.

My config below: 

Patryk_Kucia_0-1759444319767.png

Patryk_Kucia_7-1759444919056.png

 

 

Patryk_Kucia_1-1759444362651.png

Patryk_Kucia_2-1759444374961.png

Patryk_Kucia_3-1759444681177.png

Patryk_Kucia_4-1759444688360.png

Patryk_Kucia_5-1759444697031.png

Patryk_Kucia_6-1759444716121.png

 

 

 

 

 

2 replies

Technical Moderator
October 3, 2025

Hello @Patryk_Kucia 


@Patryk_Kucia wrote:

I immediately get an interrupt reporting a DMA error (128 eror code in decimal).


Please could you specify which flag that generate this?

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Associate III
October 3, 2025

HI 
IDK if it's what you meant but i did it like this :

	void HAL_SAI_ErrorCallback(SAI_HandleTypeDef *hsai)
	{
		printf("SAI error: 0x%08lx\n", hsai->ErrorCode);
		 if (hsai->ErrorCode & HAL_SAI_ERROR_OVR) printf(" -> Overrun error\n");
		 if (hsai->ErrorCode & HAL_SAI_ERROR_UDR) printf(" -> Underrun error\n");
		 if (hsai->ErrorCode & HAL_SAI_ERROR_DMA) printf(" -> DMA transfer error\n");
		 if (hsai->ErrorCode & HAL_SAI_ERROR_TIMEOUT) printf(" -> Timeout error\n");
	}

and got:

-> DMA transfer error

so i went deeper:

 if (hsai->ErrorCode & HAL_SAI_ERROR_DMA)
		 {
		 if (hsai->hdmarx != NULL)
		 printf(" -> DMA RX error: 0x%08lx\n", hsai->hdmarx->ErrorCode);
		 if (hsai->hdmatx != NULL)
		 printf(" -> DMA TX error: 0x%08lx\n", hsai->hdmatx->ErrorCode);
		 }

 and interestingly enough I got:

DMA TX error: 0x00000001

#define HAL_DMA_ERROR_TE (0x00000001U) /*!< Transfer error */

but why is there a sending error if I only want to save?

Technical Moderator
October 3, 2025

Hello @Patryk_Kucia 

Could you please share your dma config?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Associate III
October 3, 2025

Patryk_Kucia_1-1759535424746.png

and simply 

 if (HAL_SAI_Receive_DMA(&hsai_BlockA4, (uint8_t*)PDM_Buffer, PDM_BUF_SIZE) != HAL_OK)
 {
 printf("SAI RX start error!\r\n");
 }
 else
 {
 printf("SAI RX started OK\n");
 }