STM32H7B3I-EVAL: Need demo codes, Wi-Fi support; Ubuntu 24.04
Hello STM Community,
I am a beginner working with the STM32H7B3I-EVAL evaluation board based on the STM32H7B3LIH6Q MCU, and I am currently setting up my development environment on Ubuntu 24.04.3 LTS.
I installed STM32CubeIDE 1.18.0 using the following installer:
st-stm32cubeide_1.18.0_24413_20250227_1633_amd64.sh.zip
I am facing a few issues and would really appreciate your guidance.
1. Need existing demo codes for STM32H7B3I-EVAL
I would like to get the existing/demo example codes available for this board, especially the examples related to the firmware version currently flashed on my board, which shows:
Firmware Version: V1.0.1
Could anyone please guide me on where to find the exact demo code corresponding to the factory-flashed board behavior, if available?
I am specifically looking for separate demo examples for:
LED
ADC
GPIO
UART
SPI
I2C
TFT/LCD
Touch
Camera
Wi-Fi
other onboard peripherals
I am using Linux Ubuntu 24.04.3 LTS, so Linux-compatible steps would be very helpful.
At the moment, I mainly need:
official demo/example codes for STM32H7B3I-EVAL
factory demo source code / equivalent example
camera test example
Wi-Fi connection troubleshooting guidance
Any links to official STM32CubeH7 packages, board example folders, or application notes would be greatly appreciated.
Thank you very much.