Skip to main content
Associate III
March 6, 2025
Solved

STM32H7S78-DK examples exceed external RAM chip APS256XXN-OBR-BG max speed

  • March 6, 2025
  • 5 replies
  • 2812 views

Hello,

in all examples for the STM32H7S78-DK - including the TouchGFX applications - the frequency for the external APS256XXN-OBR-BG PSRAM is set to 200 MHz:

extmem_list_config[1].PsramObject.psram_public.FreqMax = 200 * 1000000u;

 

But in the datasheet for the APS256XXN-OBR-BG, see

https://www.mouser.at/datasheet/2/1127/APM_PSRAM_OPI_Xccela_APS256XXN_OBRx_v1_0_PKG-1954780.pdf

it says that the default maximum read and write clock is 133Mhz, see page 16 and 18:

rk_iot_2-1741260144048.png

It also says:

"Write latency, WLC, is default to 5 after power up. Use MR Write to set write latencies according to write
latency table. When operating frequency exceeding Fmax listed in the table will result in write data corruption."

 

Could the be a potential bug in the memory configuration of the STM32H7S78-DK board, which could lead to RAM corruption?

 

Thank you and best regards

rk_iot

 

Best answer by Dor_RH

Hello @rk_iot,

The fix has been published on GitHub. You can find it here:

[PRJ] Update PSRAM Configuration in the STM32H7S78-DK Examples to fit… · STMicroelectronics/STM32CubeH7RS@5f0b356

I hope my answer has helped you. When your question is answered, please select this topic as the solution that answered you, as it will help others find that answer faster.

Thanks for your contribution.

Dor_RH

5 replies

ST Employee
March 6, 2025

Hello @rk_iot,

Could you please provide the names of the examples you are currently working on within STM32CubeH7RS?

Thank you for your collaboration.

Dor_RH

rk_iotAuthor
Associate III
March 6, 2025

Hello @Dor_RH

All examples using external RAM are using the same settings, see:

1) STM32Cube_FW_H7RS_V1.1.0\Projects\STM32H7S78-DK\Applications\USB_Host\MSC_RTOS\Boot\Src\ extmem_manager.c:

extmem_list_config[1].PsramObject.psram_public.FreqMax = 200 * 1000000u;

 

2) STM32Cube_FW_H7RS_V1.1.0\Projects\STM32H7S78-DK\ Templates\Template_LRUN\Boot\Src\ extmem_manager.c:

extmem_list_config[1].PsramObject.psram_public.FreqMax = 200 * 1000000u;

 

3) Also when creating an Project in TouchGFX 4.24.2 Designer for the STM32H7S78-DK in the created file:

PROJECT_DIR\Boot\Core\Src\extmem_manager.c:

extmem_list_config[1].PsramObject.psram_public.FreqMax = 200 * 1000000u;

 

Best regards,

rk_iot

rk_iotAuthor
Associate III
April 15, 2025

Hello @Dor_RH 

 

Any updates on that issue? We saw that a new CubeMX Version STM32Cube_FW_H7RS_V1.2.0 was released in the meantime, but the external RAM frequency is still set to 200 MHz although the Datasheet clearly states a maximum of 133 MHz as default value.

 

This will probably lead to RAM corruption under some working conditions (high/low temperature environment, etc.).

 

We would be very thankful if you could look into this soon.

 

Thank you and best regards

rk_iot

ST Employee
April 15, 2025

Hello @rk_iot,

I reported this internally.

Internal ticket number: 207806 (This is an internal tracking number and is not accessible or usable by customers).

We appreciate your contribution.

Dor_RH

rk_iotAuthor
Associate III
May 14, 2025

Hello @Dor_RH ,

are there any updates on that internal ticket?

Thank you and best regards

rk_iot

 

ST Employee
May 14, 2025

Hello @rk_iot,

The issue is currently under investigation by the concerned team.

Thank you for your understanding and contribution.

Best regards,

Dor_RH

rk_iotAuthor
Associate III
July 11, 2025

Hello @Dor_RH 

do you have any updates on that issue by the concerned team? Would be great to know what is the expected time frame to resolve that issue, as we are considering using STM32H7S78 in our design.

Thank you and best regards,

rk_iot

ST Employee
July 16, 2025

Hello @rk_iot,

The issue has been resolved internally, and the fix will be available as soon as possible. We will keep you informed once the update is ready.

Thank you for your understanding and patience.

Dor_RH