Skip to main content
FB__1
Associate III
July 5, 2025
Solved

STM32N6 H264 video encoder and streaming over RTSP

  • July 5, 2025
  • 1 reply
  • 2161 views

Hello,

 

I would like to know the H264 VENC performance for the STM32N6 using the ST example: STM32Cube_FW_N6_V1.1.1/Projects/STM32N6570-DK/Applications/VENC/VENC_RTSP_Server

I have a hardware setup with a nucleo-n657x0-q + a ST B-CAMS-IMX camera module.

Question 1: The example provided by the STM32CUBE_FW is for STM32N6570-DK. Will it also work for the nucleo-n657x0-q 

 

Thank you.

Best answer by KDJEM.1

Hello @FB__1 ;

 

The VENC IP, integrated into the STM32/N6 device, provides hardware acceleration for H.264 and JPEG encoding.

For more information about the performance, I recommend you to look at 

KDJEM1_0-1751968285826.png

The VENC_RTSP_Server application runs on STM32N657xx devices. This application has been tested with STMicroelectronics STM32N6570-DK boards Revision MB1939-N6570-A03 and can be easily tailored to any other supported device and development board.

I hope this answer your request.

Thank you.

Kaouthar

1 reply

KDJEM.1
KDJEM.1Best answer
Technical Moderator
July 8, 2025

Hello @FB__1 ;

 

The VENC IP, integrated into the STM32/N6 device, provides hardware acceleration for H.264 and JPEG encoding.

For more information about the performance, I recommend you to look at 

KDJEM1_0-1751968285826.png

The VENC_RTSP_Server application runs on STM32N657xx devices. This application has been tested with STMicroelectronics STM32N6570-DK boards Revision MB1939-N6570-A03 and can be easily tailored to any other supported device and development board.

I hope this answer your request.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Will_Robertson
Associate III
December 23, 2025

Hi Kaouthar @KDJEM.1 

Thank you very much for the links - it's very helpful to read these. :)

Will