Associate
March 24, 2026
Question
stm32n6 usbd composite cdc+uvc failed to enumerate under windows
- March 24, 2026
- 3 replies
- 291 views
Hi,
The project was created in stm32mx from the example project cortexm_sysk.
It was generated as a CMake project and developed using VS Code.
The "USB Device Middleware Library MCU Software Component" library, version "V2.11.4 / 11-April-2025", was manually added.
CDC alone OK
UVC alone OK
CDC/HID OK
CDC/UVC NOT OK
See file in attachment.
I noticed the file descriptor is large (239 bytes). Is that a problem?
Is there another setting I need to change?
Regards,
Sébastien