STM32N657X0-Q BSEC Secured State - Cannot boot FSBL with unsigned binary
Hi ST Support Team,
I'm developing a simple FSBL application (LED control) on a NUCLEO-N657X0-Q board to understand the boot management flow with FSBL and application separation.
What I've done:
- Successfully tested the application running directly from RAM via debugger
- Compiled the FSBL for external XSPI flash (linker configured for execution from AXISRAM2 at 0x34180400)
- Signed the binary using STM32_SigningTool_CLI with header v2.3, -nk flag (no keys), -of 0x00000000, and correct load address/entry point
- Programmed the signed binary to external flash at 0x70000000 using STM32CubeProgrammer with the appropriate external loader
- Configured BOOT0=LOW, BOOT1=LOW for boot from XSPI flash
The problem: The Boot ROM does not load the FSBL into RAM. When I read AXISRAM2 (0x34180000) after reset, it contains all zeros, indicating the Boot ROM is rejecting or not attempting to load the FSBL.
What I discovered: In STM32CubeProgrammer → OTP MPU tab, I see:
- BSEC State: Secured
- Global State: 0x00000001
Additionally, from the BSEC registers:
- BSEC_SR.NVSTATE = 0xD (Secured lifecycle state)
- BSEC_HDPLSR.HDPL = 0x51
My questions:
- Is the board locked permanently? The board was brand new from the distributor. I did not intentionally configure it to Secured state during my development.
- Can I revert to Open/Development state to allow unsigned FSBL binaries for development purposes? Or is this an irreversible OTP configuration?
- Is there a development bypass mode or debug authentication procedure that would allow me to boot unsigned FSBL while in Secured state?
- Could the problem be elsewhere? The signed binary header appears valid when checked with STM32_SigningTool_CLI -dump, and the vector table in flash is correct (Stack Pointer = 0x34200000, Reset Handler = 0x34181B1D).
I need to understand if:
- The BSEC Secured state is the root cause preventing boot
- There's a way to transition back to a development-friendly state
- I should use signed binaries with real keys even for development
Any guidance would be greatly appreciated. Thank you!
Board information:
- NUCLEO-N657X0-Q
- Device: STM32N657
- Revision: Rev B
- ST-Link FW: V3J16M8
- STM32CubeProgrammer: v2.21.0