Skip to main content
Associate II
November 15, 2025
Question

STM32N657X0 SAI configuration / No clock output

  • November 15, 2025
  • 3 replies
  • 327 views

Hey,
I tried to follow all the steps of this thread as good as possible. Still I have a faulty SAI Perpheral. The Problem is that the generatet FSYNC and BCK are too low. They are both also dependent on the PLL Frequency. For example if i set IC7 so that it has 12.288MHz the FSYNC is 2kHz (insted of 48kHz) and BCK is 512kHz (instead of 12.288 MHz).
When i set IC7 to 192MHz FSYNC is 31.3kHz and BCK is about 8MHz. Also if I set any other clock channel than IC7 to feed the SAI1 Peripheral, then there won't be any FSYNC or BCK anymore.  

The D-Cache is working and doesn't give me an error as i followed this post: https://community.st.com/t5/stm32-mcus-embedded-software/stm32n6-using-dcache-with-freertos-and-sai-gpdma-usage/m-p/850823/highlight/true#M69398

I am running everything in Appli. Here are the settings:

SAI Setting:

semmelrinde_0-1763202496751.png

 

GPDMA1 Setting:

semmelrinde_1-1763202598101.png

 

3 replies

AScha.3
Super User
November 15, 2025

Hi,

i moved your post, because you posted it in response to someone else's question; now here its your question.

+

Please explain: what you want connect to SAI and what should it do ?

- Because : free format, 256bit frame, 8 slots - no idea, what this should be.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
November 15, 2025

Hi,

thank you for organizing it and your message. 

The SAI is used for reciving 8 audio channels form two 4 Channel ADCs that work together. The ADCs are Slaves. I once managed to get something similar working on a H7 but the N6 still is a challenge.
Nevertheless it also behaves like described above when I only configure it to two channels. Either way the ADCs are currently not connected and I would first of all just like the peripheral to work as expected.

November 15, 2025

Here is a short answer you can post:


Your FSYNC/BCK are wrong because SAI1 is not receiving the correct kernel clock. On STM32N6 you must configure RCC → SAI12CKSELR.SAI1SRC manually; enabling only SAI1EN is not enough.
If IC7/IC8 are not fully enabled in audio mode + divider chain, SAI falls back to a very low clock → exactly the 1/24 scaling you see (2 kHz instead of 48 kHz, 512 kHz instead of 12.288 MHz).

Also check your frame length / slot config, because a wrong FRL (e.g., 768 bits) also divides FSYNC.

Fix:

  1. Set SAI1SRC properly.

  2. Enable IC7 audio mode + divider fully.

  3. Set frame length = 256 bits, slot = 32 bits.

After correcting the kernel clock + frame length, FSYNC and BCK will output the correct frequencies.

Associate II
November 15, 2025

Hey just a quick update: Moving SAI and GPDAM1 to FSBL made the peripheral work exactly as expected. But shouldn't it be in the Appli part of the programm?