STM32N6DK750 discovery kit with SD card and camera
Hi!
I’m asking for your recommendations :
I would like to integrate the DCMIPP continuous example to add a photo capture and recording feature to the SD card through a button.
I have already configured the SD card using CubeMX, and now I want to integrate the DCMIPP continuous example and then continue adding my own contributions.
Is there another example that would be more appropriate to use as a base?
Because I prefer to use CubeMX, but with the DCMIPP example I find myself having to manually add all the libraries to my project < as it comes without cubemx>, and at the moment I see that some libraries are not recognized despite that I added them with all the paths.
Do you have any suggestions for what I want to do?
Thanks in advance