Skip to main content
Associate
June 17, 2025
Question

STM32U575 Wakeup from UART in stop mode 1

  • June 17, 2025
  • 4 replies
  • 936 views

Hi all,

I've been struggling so much to get wake from uart working on this board. 

It looks like it should be simple, I have this code which I am pretty sure should be everything needed, but it just doesn't wake up when I send data to the serial port.

Can anyone see what I might be missing?

#include <Arduino.h>
#include <stm32u5xx_hal.h>
#include <stm32u5xx_ll_usart.h>
#include <stm32u5xx_ll_bus.h>
#include "CustomPinsHub.h"
static constexpr uint32_t LED_PIN = LED1_GRN;
uint8_t aRxBuffer[10];

void SystemClock_Config(); // forward

HardwareSerial stlinkSerial(rx_pin2debug, tx_pin2debug);

void setup()
{
 stlinkSerial.begin(115200);
 HAL_PWREx_EnableUltraLowPowerMode();
 pinMode(LED1_GRN, OUTPUT);
 digitalWrite(LED1_GRN, LOW);
 stlinkSerial.println("→ Setup complete. LED is ON.");
 delay(500);
 UART_HandleTypeDef *huart = stlinkSerial.getHandle();
 UART_WakeUpTypeDef wudata{};
 wudata.WakeUpEvent = UART_WAKEUP_ON_READDATA_NONEMPTY;
 HAL_UARTEx_StopModeWakeUpSourceConfig(huart, wudata);
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_UART_ENABLE_IT(huart, UART_IT_WUF);
 HAL_UARTEx_EnableStopMode(huart);
 HAL_UART_Receive_IT(huart, (uint8_t *)aRxBuffer, 10);
 stlinkSerial.println("Entering STOP-1, waiting for any RX data to wake me..");
 stlinkSerial.flush();
 delay(500);
 HAL_SuspendTick();
 HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
 HAL_ResumeTick();
 SystemClock_Config();
 delay(500);
 stlinkSerial.println("✔ Woke up from STOP-1! Led off");
 delay(500);
 digitalWrite(LED_PIN, HIGH);
}

void loop()
{
 // nothing
}

 

4 replies

Technical Moderator
June 17, 2025
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Alan01252Author
Associate
June 17, 2025

Thanks for the swift reply, but I amm very confused, I can't see anything I am missing in that example and what the code above.. Other than 

 

EXTI10_Wakeup_Enable

 

but that doesn't actually seem to have any implementation behind it?

Technical Moderator
June 17, 2025

Try to make UART receive work before implementing the stop and waking up mode.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Andrew Neil
Super User
June 17, 2025

Arduino questions should go here: https://www.stm32duino.com/

Or, perhaps, in that main Arduino forums: https://forum.arduino.cc/ 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Alan01252Author
Associate
June 17, 2025

Thanks guys.

 

This isn't really an Arduino question, I've just cheated slightly by using the HardwareSerial abstraction, but I'll remove that if it makes this thread clearer and just go-to pure HAL.

 

I have tried changing the clock via HAL but perhaps I've done something wrong there 

Andrew Neil
Super User
June 17, 2025

@Alan01252 wrote:

using the [Arduino] HardwareSerial abstraction, 


Maybe that's what's causing the problem?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Alan01252Author
Associate
June 18, 2025

Thanks all, I really appreciate the effort of you all reviewing this :)

I still can't get this working, I think my next step is to use a scope and see what's happening as I don't believe the code is "missing" anything now. At least nothing obvious..

My latest iteration I think is as simple as it can get...

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file UART/UART_WakeUpFromStopUsingFIFO/Src/main.c
 * @author MCD Application Team
 * @brief This sample code shows how to use UART HAL API (UART instance)
 * to wake up the MCU from STOP mode using the UART FIFO level.
 * Two boards are used, one which enters STOP mode and the second
 * one which sends the wake-up stimuli.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <CustomPinsHub.h>
#include <stm32u5xx_hal.h>
#include <stm32u5xx_hal_gpio.h>
#include <stm32u5xx_ll_usart.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
#define HAL_TIMEOUT_VALUE 0xFFFFFFFF
#define countof(a) (sizeof(a) / sizeof(*(a)))
/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart3;

/* USER CODE BEGIN PV */
uint8_t HeaderTxBuffer[] = "\r\nUSART3 WakeUp from stop mode using FIFO\r\n";
uint8_t Part1TxBuffer[] = "\r\n\t Part 1: RXFIFO threshold interrupt\r\n Waiting for characters reception until RX FIFO threshold is reached\r\n Please send 2 bytes\r\n";
uint8_t WakeupRXFTBuffer[] = "\r\n Proper wakeup based on RXFIFO threshold interrupt detection.\r\n";
uint8_t Part2TxBuffer[] = "\r\n\t Part 2: RXFIFO full interrupt\r\n Waiting for characters reception until RX FIFO is Full \r\n Please send 8 bytes\r\n";
uint8_t WakeupRXFFBuffer[] = "\r\n Proper wakeup based on RXFIFO full interrupt detection.\r\n";
uint8_t FooterTxBuffer[] = "\r\nExample finished successfully\r\n";

uint8_t RxBuffer[8];
/* USER CODE END PV */

static void SystemPower_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
/* USER CODE BEGIN PFP */
static void EXTI11_Wakeup_Enable(void);

void SystemClock_Config_fromSTOP(void);
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

void HAL_MspInit(void)
{
 /* USER CODE BEGIN MspInit 0 */

 /* USER CODE END MspInit 0 */

 __HAL_RCC_PWR_CLK_ENABLE();

 /* System interrupt init*/

 /* USER CODE BEGIN MspInit 1 */

 /* USER CODE END MspInit 1 */
}

void USART3_IRQHandler(void)
{
 HAL_UART_IRQHandler(&huart3);
}

int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 __HAL_RCC_HSI_ENABLE();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* Configure the System Power */
 SystemPower_Config();

 /* USER CODE BEGIN SysInit */
 /* Initialize BSP LED */
 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();

 MX_USART3_UART_Init();

 HAL_UARTEx_EnableFifoMode(&huart3);
 HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_4); // 2 bytes
 HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8);

 /* USER CODE BEGIN 2 */
 __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI);

 const char *test = "USART3 alive!\r\n";
 HAL_UART_Transmit(&huart3, (uint8_t *)test, strlen(test), HAL_MAX_DELAY);

 // const char *echoBanner = "\r\n--- UART Echo Test ---\r\n"
 // "Type characters, they will be echoed back.\r\n"
 // "Send 'S' (0x53) to skip to STOP-mode test.\r\n";
 // HAL_UART_Transmit(&huart3, (uint8_t *)echoBanner, strlen(echoBanner), HAL_MAX_DELAY);

 // uint8_t ch;
 // while (1)
 // {
 // if (HAL_UART_Receive(&huart3, &ch, 1, HAL_MAX_DELAY) == HAL_OK)
 // {
 // HAL_UART_Transmit(&huart3, &ch, 1, HAL_MAX_DELAY);
 // if (ch == 'S') // user requests to move on
 // break;
 // }
 // }

 UART_WakeUpTypeDef wakeup = {
 .WakeUpEvent = UART_WAKEUP_ON_READDATA_NONEMPTY};
 if (HAL_UARTEx_StopModeWakeUpSourceConfig(&huart3, wakeup) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_RCC_HSISTOP_ENABLE();
 HAL_UART_Transmit(&huart3, (uint8_t *)&HeaderTxBuffer, countof(HeaderTxBuffer) - 1, HAL_TIMEOUT_VALUE);
 HAL_UARTEx_EnableStopMode(&huart3);
 EXTI11_Wakeup_Enable();
 HAL_UART_Transmit(&huart3, (uint8_t *)&Part1TxBuffer, countof(Part1TxBuffer) - 1, HAL_TIMEOUT_VALUE);
 HAL_UART_Receive_IT(&huart3, (uint8_t *)&RxBuffer, 1);
 HAL_SuspendTick();

 HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);

 HAL_ResumeTick();
 SystemClock_Config();
 HAL_UARTEx_DisableStopMode(&huart3);
 HAL_UART_Transmit(&huart3, (uint8_t *)&WakeupRXFTBuffer, countof(WakeupRXFTBuffer) - 1, HAL_TIMEOUT_VALUE);
 const char *testEnd = "USART3 alive again!\r\n";
 HAL_UART_Transmit(&huart3, (uint8_t *)testEnd, strlen(testEnd), HAL_MAX_DELAY);
 HAL_Delay(100);

 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
}

/**

/**
 * @brief Power Configuration
 * @retval None
 */
static void SystemPower_Config(void)
{

 /*
 * Disable the internal Pull-Up in Dead Battery pins of UCPD peripheral
 */
 HAL_PWREx_DisableUCPDDeadBattery();
 /* USER CODE BEGIN PWR */
 /* USER CODE END PWR */
}

/**
 * @brief USART1 Initialization Function
 * None
 * @retval None
 */
static void MX_USART3_UART_Init(void)
{

 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART3;
 PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_HSI;
 HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit);

 __HAL_RCC_USART3_CLK_ENABLE();

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 huart3.Instance = USART3;
 huart3.Init.BaudRate = 115200;
 huart3.Init.WordLength = UART_WORDLENGTH_8B;
 huart3.Init.StopBits = UART_STOPBITS_1;
 huart3.Init.Parity = UART_PARITY_NONE;
 huart3.Init.Mode = UART_MODE_TX_RX;
 huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart3.Init.OverSampling = UART_OVERSAMPLING_16;
 huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_EnableFifoMode(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */
}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */
 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 GPIO_InitStruct.Pin = GPIO_PIN_10 | GPIO_PIN_11;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */
 /* USER CODE END MX_GPIO_Init_2 */
 HAL_NVIC_SetPriority(USART3_IRQn, UART_IRQ_PRIO, UART_IRQ_SUBPRIO);
 HAL_NVIC_EnableIRQ(USART3_IRQn);
}

/* USER CODE BEGIN 4 */
static void EXTI11_Wakeup_Enable(void)
{
 EXTI_HandleTypeDef hexti;
 EXTI_ConfigTypeDef exticonfig;
 exticonfig.Line = EXTI_LINE_11;
 exticonfig.Mode = EXTI_MODE_INTERRUPT;
 exticonfig.Trigger = EXTI_TRIGGER_RISING;
 exticonfig.GPIOSel = EXTI_GPIOC;
 HAL_EXTI_SetConfigLine(&hexti, &exticonfig);
}
Alan01252Author
Associate
June 19, 2025

Last ditch bump as a cry for help :) Myself and a colleague have basically tried everything we can think of now, but aren't any closer to getting this working.

MM..1
Chief III
June 19, 2025
Technical Moderator
June 25, 2025

Hello @Alan01252 

Any update for this issue?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"