stm32u575vgt, usart DMA rX , rx_buff was not changed by DMA.
Post edited by ST moderator. In next time please use </> to share your code. Thank you for your understanding.
hi, I am using stm32U5's uasrt2 DMA RX , DMA interrupt coming, usart idle int coming, ROR value right, but rx_buffer was not refreshed by DMA, here is my part of code.
/* USER CODE BEGIN PV */
uint8_t loop_TX = 0xaa;
uint8_t loop_RX = 0x0f;
/* USER CODE END PV */
.............................
/* MPU Configuration--------------------------------------------------------*/
MPU_Config();
/* Reset of all peripherals, Initializes the Flash interface and the Systick.
*/
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* GTZC initialisation */
MX_GTZC_Init();
/* USER CODE BEGIN SysInit */
delay_init();
HAL_Delay(100);
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_GPDMA1_Init();
MX_SPI2_Init();
MX_USB_OTG_FS_PCD_Init();
MX_UCPD1_Init();
MX_I2C4_Init();
MX_LPUART1_UART_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
MX_I2C3_Init();
MX_FLASH_Init();
MX_TIM2_Init();
MX_USART1_UART_Init();
MX_ICACHE_Init();
/* Initialize interrupts */
MX_NVIC_Init();
HAL_Delay(100);
while (1) {
/* First transmit data, then start DMA receive */
if (loop_TX < 0xFF) {
loop_TX++;
HAL_UART_Transmit(&huart2, &loop_TX, 1, 100);
HAL_Delay(100);
/* Start DMA receive with IDLE detection */
HAL_UARTEx_ReceiveToIdle_DMA(&huart2, &loop_RX, 1);
/* Wait for DMA transfer to complete */
HAL_Delay(500);
/* Flush cache to ensure DMA data is visible to CPU */
//SCB_InvalidateDCache_by_Addr(&loop_RX, sizeof(loop_RX));
printf("[MAIN] TX: %02X, RX: %02X\r\n", loop_TX, loop_RX);
}
}
void USART2_IRQHandler(void)
{
/* USER CODE BEGIN USART2_IRQn 0 */
if (__HAL_UART_GET_FLAG(&huart2, UART_FLAG_IDLE)) {
__HAL_UART_CLEAR_IDLEFLAG(&huart2);
uint16_t dma_cntr = __HAL_DMA_GET_COUNTER(huart2.hdmarx);
/* Flush cache to ensure DMA data is visible to CPU */
//SCB_InvalidateDCache_by_Addr(&loop_RX, sizeof(loop_RX));
printf("[USART2] IDLE, DMA CNDTR=%u, RX=%02X, RDR=%02X\r\n",
dma_cntr, loop_RX, huart2.Instance->RDR);
}
/* USER CODE END USART2_IRQn 0 */
HAL_UART_IRQHandler(&huart2);
/* USER CODE BEGIN USART2_IRQn 1 */
/* USER CODE END USART2_IRQn 1 */
}
void GPDMA1_Channel4_IRQHandler(void)
{
/* USER CODE BEGIN GPDMA1_Channel4_IRQn 0 */
/* USER CODE END GPDMA1_Channel4_IRQn 0 */
HAL_DMA_IRQHandler(&handle_GPDMA1_Channel4);
/* USER CODE BEGIN GPDMA1_Channel4_IRQn 1 */
printf("[GPDMA1_Channel4] DMA done, CNDTR=%u\r\n",
__HAL_DMA_GET_COUNTER(&handle_GPDMA1_Channel4));
printf(
"[GPDMA1_Channel4] DMA buf: %02X %02X %02X %02X %02X %02X %02X %02X\r\n",
g_oas1200.rx_buffer[0], g_oas1200.rx_buffer[1], g_oas1200.rx_buffer[2],
g_oas1200.rx_buffer[3], g_oas1200.rx_buffer[4], g_oas1200.rx_buffer[5],
g_oas1200.rx_buffer[6], g_oas1200.rx_buffer[7]);
/* USER CODE END GPDMA1_Channel4_IRQn 1 */
}here is some print result :
[MAIN] loop_RX addr=0x20000029
[GPDMA1_Channel0] DMA done, CNDTR=0, CSAR=0x40004424, CDAR=0x20000029, CTR1=0x00000000
[MAIN] TX: B4, RX: 0F
[USART2] IDLE, DMA CNDTR=0, RX=0F, RDR=B5
[MAIN] loop_RX addr=0x20000029
[GPDMA1_Channel0] DMA done, CNDTR=0, CSAR=0x40004424, CDAR=0x20000029, CTR1=0x00000000
[MAIN] TX: B5, RX: 0F
[USART2] IDLE, DMA CNDTR=0, RX=0F, RDR=B6[MAIN] loop_RX addr=0x20000029
[GPDMA1_Channel0] DMA done, CNDTR=0, CSAR=0x40004424, CDAR=0x20000029, CTR1=0x00000000


I connect usart2 TX and RX pin to do the test , the RX value should be equal to TX, I have no idea what is wrong ....